Skip navigation
B Mimic Bhairav Pardiwala       First A Note Towards Contest Folks:- Hello folks this is my 2nd entry into Azure Sphere contest (I have logged my first entry B Inventory  into a different account but both of these accounts are mine! Please take both entries into consideration while judging!) Now onward's to my second entry :-).   Description:- Many a times it happens in retail that a shop may not have a certain piece or part but the consumer would very much like to see ...
  (This project should use latest 3+1909 beta SDK and OS 19.10) Introduction Let's Begin PM2.5 sensor Driver Intercore message facilities BME680 and BSEC LTC1695 LED Storage Web Interface Connect IOS/Android though http server Azure IoT Central Summary Source Code Introduction This is my experiment of using Azure Sphere kit for the Sensing the World Phase 2. This is a project that sense the air quality and control the fan speed for ...
Overview  Lately there is a haze hazard happening in Malaysia. I thought of doing the air quality project using the Azure Sphere MT3620 Starter Kit.  While researching on doing the project, I found out that I do not have the air quality sensor to use with the Azure Sphere.  Hence I change it to this project which I use the onboard temperature sensor and a relay click board.     Features The idea is simple.  The context is my home where I want to keep it comfortable ...