Skip navigation

Azure Sphere

November 30, 2019
1. Introduction   The project was born from the need to have a universal charger that is able to charge both 1 cell and a battery pack for child car or scooter . The main concept to make Li-ion charger was using the block for fast prototyping. I chose as hardware for this role 5 modules: 1. MT3620 2. LM2596 3. INA226 4. MCP4725 5. OLED Display 2. Description of concept     On the diagram bellow are present the connection between all additional boards.   The ...
Background This project uses the Azure Sphere MT3620 Starter Kit to convert a CO2 sensor into an IoT device. The world is becoming increasingly aware that carbon dioxide is the primary greenhouse gas (accounting for about two thirds of greenhouse heating) and it has been steadily increasing its concentration in air since the industrial revolution began. In the last 100 years it has increased from its pre-industrial peak of about 300 ppm to 415 ppm today (you can check it here: https://www.co2.e ...
Hello, This is my entry for the "Sensing the World" challenge. This project is completely open-source: both of the firmwares and the mobile app for viewing the logged data are available on GitHub (firmware and app).   This project is meant to be a tool to better analyze fuel consumption of your car based on the routes you take for moving and commuting. By combining data from a GPS receiver (connected to a standard 9600 baud simplex UART with NMEA protocol) and an OBDII interface (anythi ...
1) Introduction Predictive analytics is the process of using data analytics to make predictions based on data. This process uses data along with analysis, statistics, and machine learning techniques to create a predictive model for forecasting future events. Digital twin technology implies creating a virtual representation of a physical asset or a system; to model its state and simulate its performance. Digital twins are continuously learning systems, powered by machine learning algorithms, whic ...
1) Introduction Predictive analytics is the process of using data analytics to make predictions based on data. This process uses data along with analysis, statistics, and machine learning techniques to create a predictive model for forecasting future events. Digital twin technology implies creating a virtual representation of a physical asset or a system; to model its state and simulate its performance. Digital twins are continuously learning systems, powered by machine learning algorithms, whic ...
Use the Azure Sphere Starter Kit and two click boards to monitor current weather conditions and send the data to the Azure Cloud. If you have just received your Azure Sphere device, make sure to follow this getting started guide to get it set up first, or else all of the steps below will fail to work. BME680 Sensor Overview It can detect temperature, humidity, pressure, and even volatile organic compounds (VOCs), such as CO2. Bosch provides a basic API, but it doesn’t play nicely with t ...
1. Introduction 1.1 Azure Sphere 2. Getting Started 2.2 Examples 3. Hardware 3.1 Avnet MT3620 Starter Kit 3.1 Plantower PMS7003 - Laser Dust Sensor 3.2 OLED Module 3.3 Enclosure 3.4 Assembly 4. Software 4.1 A7 High Level Application 4.2 M4 Real Time Application 4.3 PMS7003 Sensor Driver 5. Azure IoT Central Application 5.1 Device Template 5.1.1 Adding a device 5.2 Measurements 5.3 Dashboard 5.4 Rules and Notifications ...
Unfortunately I found out about this project much too late. I first signed up on Nov, 10, 2019. I not even sure I will have phase 1 completed before the dead line but I figure what the heck, I am going to keep plugin away at it   So I order the kit and got it and got though the first two blogs on setting it up and getting it connected. I determined a project that I wanted to accomplish and order the parts. I am hoping that maybe the date for phase two will somehow get pushed out. If not I ...
Monitor the health of the vehicle and diagnose any potential problem securely, using Azure Sphere and Microsoft Azure cloud services.1. Problem StatementThink about a perfectly normal day of your life. You are following all of your daily routines, happily and then suddenly you have a "heart attack". When you gain consciousness you are already in an operation theater surrounded by doctors in the green gown with a mask on their face, ready to operate. You found out that there are multiple blockage ...
vinojv

Sphere

Posted by vinojv Nov 30, 2019
Continuing my work on sphere ...