Skip navigation

Azure Sphere

2 Posts authored by: saicheong
A simple web server for Azure Sphere w/ demo for change wifi setting via web server Install    Simple clone it and complie at visual studio.     Running    The programe start at SSID: First and Open network (No password), so the device try to connect to AP as open network with SSID First.     Change of WIFI network is easy, just access ip:8080 on browser, select new network, put psk password and click submit.     To Reset the wifi, click RE ...
  (This project should use latest 3+1909 beta SDK and OS 19.10) Introduction Let's Begin PM2.5 sensor Driver Intercore message facilities BME680 and BSEC LTC1695 LED Storage Web Interface Connect IOS/Android though http server Azure IoT Central Summary Source Code Introduction This is my experiment of using Azure Sphere kit for the Sensing the World Phase 2. This is a project that sense the air quality and control the fan speed for ...