Skip navigation
We get asked from time to time whether you can use BitScope with Windows 98, XP and Vista. The short answer is yes but your mileage may vary. Here is the latest edition (as at the time of writing) of BitScope DSO running on Windows XP: Unfortunately we can no longer provide official support for these old versions of Windows but we'll do our best to ensure you can still use them. No point to throwing away that ancient but otherwise useful Windows PC or notebook, turn it into a Mixed Signal Osci ...
SPI – Serial Peripheral Interface Demystified This article cross-posted from Raspi.Tv with permission and our thanks! I was in need of an interesting signal to check out the logic analyser functionality of the BitScope micro. So, another of my current RasPiO® Beta boards was used as a convenient way to connect an mcp3008 analog to digital converter (ADC) to the Pi and the scope. RasPiO Analog board + BitScope probes connected I don’t claim to be an expert on SPI, but having ...
We've released the first beta update in the development branch ahead of BitScope DSO version 3.0. DSO 2.9 Ready NowWe've been collecting your feedback as we work towards the release of DSO 3.0. We have added new features and fixed many bugs. The time has come to make the new version available for beta testing. We want you to have the latest software for BitScope as soon as possible. This means releasing the new version it while it's still in development. This software fixes many bugs reported i ...