Skip navigation
The Pmod ESP32 provides an easy and cost-effective way to add wireless communication to any host platform or project. It uses the fully certified ESP-WROOM-32 Wi-Fi + BLE + BT module from Espressif Systems. Pmod ESP32 is suitable for a wide variety of applications, from low-power sensor networks to more demanding tasks such as music streaming. It was designed in collaboration with Renesas and is supported by all Renesas Synergy Platforms.     Key features: Wi-Fi, Bluetooth LE, and ...
  The Arty A7-100T contains a Xilinx XC7A100T FPGA which is the largest FPGA available for the Arty A7 and is ideal for deployment of softcore processors. These processors can be either proprietary or open-source. One of the most popular open source processors is the RISC-V.   This tutorial covers building a RISC-V processor, specifically the SiFive Freedom E310 and steps through the process of loading the Freedom E310 onto an Arty A7, and programming it using the Arduino IDE.   ...