Skip navigation
ARM MCU should have an external parallel bus interface to be connected to the graphics controller. Please visit http://www.colibrigraphics.com/ to see a list of ARMs with this peripheral. ...
Looking for faster & free embedded GUI design ?   The Graphics Display Designer tool enables graphical design of the user interface and generates C code which can be directly compiled into libray calls using the free Microchip compilers. Code can then be tested using the Graphics development kits based on PIC24F/H, dsPIC33 or PIC32 processors. For highest integration, PIC24F family with on-chip graphics LCD controller can be used and developed with the new PIC24FJ256DA210 Development ...
Please visit http://www.colibrigraphics.com to seach a TFT glass for your project. ...
Free Epson S1D13781 Configuration Utility generates an initial code for the graphics controller. It can be downloaded from http://www.colibrigraphics.com ...
The first Embedded Systems Conference in Chicago (well, truth be told, Rosemont,  IL, which is just off the runway at O’Hare) was “co-located” this week with the somewhat larger Sensors Expo & Conference. The notion of co-location doesn’t always succeed—you would probably not want to be co-located in the same house with your neighbor, for example—but since sensors play a key role in embedded technology, especially in the automotive and industrial spac ...

Filter Blog

By date: By tag: