Skip navigation
  Samsung has taken DRAM to a whole new level, 12.8GB/sec, a great increase over the former LPDDR2. In the process, reducing power consumption by 87%. The increase in data transmission is due to the increase of I/O pins to 512 from the 32 the prior gen memory used. Currently at 1Gb, Samsung plans to release 4Gb modules by 2013. We should see the introduction of this memory in Samsung's future tablets and cell phones. Samsung also hopes to be at the forefront of the DRAM memory demand of a s ...
A complete computer system in 1 cubic millimeter. Onboard is a low power microcontroller, memory, battery, wireless radio, solar cell, and a pressure sensor. This system is meant to be an implantable eye pressure monitor for glaucoma patients. I'm sure a patient would feel this think, despite the size. Think about getting a splinter. Created by three professors from the University of Michigan, Dennis Sylvester, David Blaauw, and David Wentzloff, the project was presented at the International Sol ...
The first (sequential) logic circuit has been built using carbon nanotubes. The fast manufacturing process has been developed to print these circuits on TFT with a plastic sub straight resulting in a flexible circuit board. Professors Yutaka Ohno from Nagoya University in Japan and Esko I. Kauppinen explained, nanotube networks contain both metallic and semiconducting nanotubes. While a greater amount of metallic nanotubes increases the transistor’s charge-carrier mobility, it also decreas ...
Faster mobile device access is close at hand. SanDisk Corporation recently announced its next generation of iNAND and iNAND Ultra embedded flash drives featuring smaller and thinner form factors. Available in packages as small as 11.5mm x 13mm x 1mm, SanDisk's new iNAND and iNAND Ultra e.MMC products support the increasing demand for slimmer and more compact smartphone and tablet designs. The company reduced its iNAND package sizes by using advanced 24nm generation NAND memory chips, which are m ...
Pelican, a California startup company, is trying to make a big name for themselves by being a little outside the box. They a promoting a new camera for cellphones that consists of 25 small cameras. The concept is to spread available light over the 25 lenses as opposed to the large one it they are replacing. Image quality is improved by this capturing of more light, and performs extremely well in low light conditions. The final imaged is a collage of the 25 smaller pictures. Pelican also boasts t ...
Engineers and scientists collaborating at Harvard University and the MITRE Corporation have developed and demonstrated the world's first programmable nanoprocessor. “This work represents a quantum jump forward in the complexity and function of circuits built from the bottom up, and thus demonstrates that this bottom-up paradigm, which is distinct from the way commercial circuits are built today, can yield nanoprocessors and other integrated systems of the future,” said Charles M. Lie ...
Graphene molecular model image. A new transistor made from graphene, the world's thinnest material, has been developed by a research team at the University of Southampton. The new transistor achieves a record high-switching performance which will make our future electronic devices, such as PDAs and computers, even more functional and high-performance. “Silicon CMOS downscaling is reaching its limits and we need to find a suitable alternative. Other researchers had looked at graphene as a ...
OK, so it can’t reach the energies produced at the LHC or Tevatron, but this is still pretty impressive. Engineers at a micro-electro mechanical systems conference that was held recently in Cancun, unveiled this tiny cyclotron device, which can speed argon ions down a 5-millimeter accelerator track. Their chip-size cyclotron can guide argon ions with around 1.5 kiloelectronvolts of energy down a 5-millimeter accelerating track before whipping them around a 90-degree turn. The system boosts ...
Recently Marvell announced the world’s first ‘ultra-low power, ultra-high performance’ 1.5 GHz three-core processor that is the first to feature 3D graphics performance with quad unified shaders for 200 million triangles per second delivered on mobile devices. According to Marvell, the Armada 628 can deliver dual stream 1080p 3D video and 3D graphics performance with quad unified shaders for 200 million triangles per second delivered on ultra-low-power, long battery life smartp ...
Gallium nitride material holds promise for emerging high-power devices that are more energy efficient than existing technologies, but these GaN devices traditionally break down when exposed to high voltages. Now researchers at North Carolina State University have solved the problem, introducing a buffer that allows the GaN devices to handle 10 times greater power. Previous research into developing high power GaN devices ran into obstacles, because large electric fields were created at specific p ...

Filter Blog

By date: By tag: