Skip navigation
Here is a short video explaining how one can create a new design for NAND Flash controller.     For more information on NAND Flash Controller, you can visit http://www.slscorp.com/pages/iponficntrlr.php   OR   Contact info@slscorp.com mentioning your query/request for information. ...
Here is a sample application that we have created using the CoreCommander board for mass storage on Altera FPGA.   The video given below does not have voice.  You can read the comments and view the mass storage implementation.   ...
Syed Abbas

Robotic arm & traxster

Posted by Syed Abbas May 19, 2011
The aim of this project is to control a Robotic Arm which is mounted on to  the Traxster.  Wii Nunchuck is used to control Robotic Arm and Traxster. We are just using the two buttons and the Joystick and this data is been transfers wirelessly using the Xbee Shield between the two  Arduinos. We are using a L298N to run the DC motors of the traxster which has been made in to the PCB. we are using 9 vold battery to power the Arduino which is in the traxaster and 12 Volt battery to po ...
Embedded software engineers only need to know one programming  language to get through life: C. Most embedded software projects are  written in C. So that leaves most other languages out of use (I insist,  for embedded programmers). I always wonder if I need to start learning a  new language, and if so, which one. With so many things to keep  learning about, I usually barely have time to read up on the latest  developments in the technologies I work with, so learnin ...
Andy_Sills

Dynamic Security Lock

Posted by Andy_Sills May 13, 2011
for my project i produced a security locking device where a new code was generated every hour. it used a one way encryption alogithm, to scramble the time and key data producing a new password. it has a number of features including admin login to generate a new key which was saved in the EEPROM, also lockdown mode if a user had three 'wrong guesses.'' the project came complete with an iphone application with the same algorithm uploaded to the code could be revealed. the algorithm was a mixurture ...
The aim of this project is to control a Robotic Arm which is mounted on to  the Traxster.  Wii Nunchuck is used to control Robotic Arm and Traxster. We are just using the two buttons and the Joystick and this data is been transfers wirelessly using the Xbee Shield between the two  Arduinos. We are using a L298N to run the DC motors of the traxster which has been made in to the PCB. we are using 9 vold battery to power the Arduino which is in the traxaster and 12 Volt battery to po ...
Going into the 2011 Embedded Systems Conference Silicon Valley I was looking forward in particular to seeing and hearing more about new MCUs and ecosystem developments.   The show did not disappoint.   If there was one product to capture “best in show” honors a good argument could be made on behalf of TI’s MSP430FR57xx, a 16-bit microcontroller said to be the industry's first low power ferroelectric random access memory (FRAM) MCU. TI has been working on FRAM te ...

Filter Blog

By date: By tag: