Skip navigation
2014
Bigger is not always better. Kinetis mini MCUs are a new category of Kinetis MCUs powered by ARM® Technology and available in a variety of tiny wafer-level chip-scale packages (WLCSPs), currently starting at just 1.9 x 2 mm2.   ...
OBsIV’s XIM4 console adapter... app based tuning is an important next step. (via XIM)   The XIM3 was amazing (see the tear-down)… does the XIM4 live up to the same standards? Ask any gamer on the planet and they will tell you there are two factions that have been raging a debate with one another over the better part of two decades concerning which platform is the best for gaming, consoles or PCs. Both have their advantages and disadvantages, consoles such as the PS4 and Xbox ...
IoT connected mailbox... or is it just a package monitor? (via kickstarter) The Internet of Things is fast approaching and many appliances and everyday objects are beginning to become connected to the internet. With the plethora of devices now available, making this happen is now easier than ever. Devices such as Arduinos have attracted people to programming and have brought more people into the do-it-yourself community, creating one of the largest communities in electronics. Due to the Ard ...
kobelo

Mr.

Posted by kobelo Jan 5, 2014
help me to connect graphical display based on ks0108 controller to the arduino how to add libraries to the proteus version 8 ...
Geomerics’ Enlighten lighting engine featured in Battlefield 4. Mobile will be able to play games.. but the HMI is still lacking! (via ARM) Gaming on mobile devices has come a long way in the last five years due to avalanche advancements in technology, which allowed us to go from playing Tetris to playing first-person shooters. There’s a good chance that the mobile device your currently using has an ARM processor in it, especially if it’s an Android-based device. Users tha ...

Filter Blog

By date: By tag: