cpulse.jpg

The cPulse is seen in action being used as a home rave device (via Codlight)


The French company, Codlight Inc. is currently seeking funding on Kickstarter to produce one of the first fully customizable LED Smartphone cases. While the prospect of becoming a walking, breathing billboard advertisement doesn't particularly appeal to me, I must give Codlight Inc. credit for the multitude of features and uses it offers.

 

The company certainly left no stone unturned when they programmed the cPulse smartphone case for a variety of uses. The cPulse LED case can act as everything from a notification banner, to a homemade rave device, to a form of light therapy. This feature can also be used to mimic a good old-fashioned analog clock radio.

 

The cPulse uses a panel of 128 high-efficiency LED lights powered by the Smartphone battery, and controlled by a custom program which allows the user to specify different commands, modes, notifications, and create customizable light shows set to music.

These light displays sap battery power at a rate of about 7% per hour so you may want to have quarters on hand if you need to call someone on short notice. - Remember payphones?

 

The LED light panel and the smartphone case  are 3D printed by Sketchfab and Sculpteo. Kickstarter backers who fund at least $79 to this Codlight initiative will receive a kit that will allow them to 3D print their very own cPulse case. Donors who are a bit more generous, funding at least $89 will receive a fully functioning cPulse case delivered to their home.

 

At the moment, the case is specifically made for the Android 4.4 smartphone, however if the project gets off of its feet, its easy customization could allow anyone to own a cPulse.

 

I must say, I am still pretty impressed by the functionality of this device, even though it is entirely unnecessary and a product of a culture of consumption and excess.

 

For now, Codlight Inc. is asking for no paltry sum, with a pledged goal of $350,000. They are currently nowhere near the goal, but still have about a month left to raise over a quarter of a million dollars.

 

If you are obsessed with bright, shiny objects and want to blind and dazzle those around you, you can get your very own cPulse from Kickstarter.



C

See more news at:

http://twitter.com/Cabe_Atwell