Click boards -- The Biggest Add-on Board Collection in the World
Posted by bhfletcher
If you've never heard or used a Click board, now is a great time to check them out.
Click Boards from MikroElektronica
MikroElektronika invented the Click boards and the mikroBUS standard to which they fit. MikroElektronika makes the claim, "The Biggest Add-on Collection in the World," and I think they are correct. As of today, November 30th 2020, I can see 974 items on their https://www.mikroe.com/click landing page, including Sensors, Displays, Wireless transceivers, Motor control, Connection ports, Encoders, speech recognition, thunder detection, and fingerprint scanning.
mikroBUS
At the heart of the Click technology is the mikroBUS -- a 12-pin, dual-row standard that includes SPI, I2C, and UART protocols, along with an Analog input and PWM output. Voltage sources of 5V and 3.3V are both accessible on the mikroBUS.
96Boards Mezzanine / Ultra96-V2
On the Avnet Ultra96-V1 or Ultra96-V2, you can adapt the 96Boards Low-speed Expansion to two mikroBUS sites using the Click Mezzanine. You can purchase the Click Mezzanine either by itself (AES-ACC-U96-ME-MEZ) or in a bundle (AES-ACC-U96-ME-SK) that includes the mezzanine plus 3 Click boards (USB UART with Microchip MCP2221, 2x16 Character LCD with Microchip controller, and 6DoF inertial measurement unit with ST Micro LSM6DSL).
For more information about the Starter Kit, see this page:
96Boards Click Mezzanine Starter Kit
For an example project using the Starter Kit, see:
Buy 96Boards Click Mezzanine Starter KitBuy 96Boards Click Mezzanine Starter Kit
Buy 96Boards Click MezzanineBuy 96Boards Click Mezzanine
Buy Ultra96-V2Buy Ultra96-V2
Buy Ultra96-V2 I-gradeBuy Ultra96-V2 I-grade
Sphere
The Azure sphere MT3620 Starter Kit has native mikroBUS sites on-board. You can read more about some of the example designs for Sphere with Click here:
Using MikroE Click Boards™ with Microsoft Sphere
Azure Sphere and Click Stepper2 Motor Control
Buy Azure Sphere Starter KitBuy Azure Sphere Starter Kit
Arduino
Any board that has an Arduino UNO or MEGA Shield interfaces can also be adapted to mikroBUS sockets, which opens up a couple other Xilinx-based boards, like MiniZed and MicroZed with the Arduino Carrier Card. Of course, a number of Arduino type boards are also compatible with these shields as well.
Buy Arduino UNO Click ShieldBuy Arduino UNO Click Shield
Buy Arduino MEGA Click ShieldBuy Arduino MEGA Click Shield
Buy MiniZedBuy MiniZed
Buy MicroZed Arduino Carrier CardBuy MicroZed Arduino Carrier Card
Raspberry Pi / MaaXBoard
MikroElektronika also offers an adapter for a Raspberry Pi Hat, which is also compatible with the Avnet MaaXBoard. Check out this blog using MaaXBoard, the Click Pi Hat, and Azure:
Sending Data to Azure with MaaXBoard
Buy Raspberry Pi Click HatBuy Raspberry Pi Click Hat
Buy MaaXBoardBuy MaaXBoard
If you're looking to quickly prototype something with your favorite development, it is definitely worth exploring mikroBUS compatibility and if you can use Click boards for your testing. Like I said at the start, it is "The Biggest Add-on Board Collection in the World!"
Comments