Skip navigation

Embedded

6 Posts authored by: kjachim
Despite the thousands of development boards that have shipped and the overwhelming interest from the market for the i.MX RT1170 crossover MCU, I do come across an occasional customer that does not understand the value.  They say they do not need the performance or integration or security that the i.MX RT1170 MCU family offers.  More often than not though, they simply do not understand how these features could work for them in their applications.   Take, for example, applications ...
The Hackster Crossover Code Challenge might be over, but really, it’s just the beginning for you. Now it’s your chance to take advantage of all the ideas to jump start your next design.   The Crossover Code Challenge generated lots of project examples using NXP’s i.MX RT1010 EVK and MCUXpresso software. All of which are available for you to leverage here. These projects include things like pictures, documentation, schematics and software and spanned applications like ...
Launched in October, the i.MX RT1010 crossover MCU further expands NXP’s popular i.MX RT series and introduces the world to the next generation of low-cost, high-performance MCUs.     With features such as Flex PWM for motor control, S/PDIF for audio, and a FlexIO module for things like graphic LCDs, it is easy to see the breadth of products and use cases that could benefit from such a general purpose, feature-rich MCU (read the i.MX RT1010 blog series here for even more ideas ...
    The eXecute in Place, or XiP, is a capability that allows a processor to execute code directly from external flash memory. Many embedded applications require connectivity stacks, audio processing, and vision, and the amount of executable code for these functions has grown to substantial sizes.  When considering these application requirements together for one embedded system, the capability of XiP with external flash is an essential enabler as it allows nearly limitless data sp ...
  Why is the package type usually one of the last considerations when selecting an MCU or processor? An inefficient package can present issues to project schedule, system performance, board size and most importantly cost.   Luckily, the i.MX RT crossover processors cater to the PCB layout engineer. In package development, we perform several pinout iterations, conduct package fan out exercises for 2-layer PCBs on our LQFP packages and 4-layer PCBs on our BGA packages and finish by act ...
kjachim

i.MX RT Saves the Day

Posted by kjachim Mar 15, 2019
  During the development of a new product, have you ever been asked at the last minute to include more features?  Add a smartphone-like GUI, make it adapt with machine learning, connect it to the cloud, and the list goes on and on.  The challenge for us engineers is that there is always a caveat – add these new features, while reducing the cost and shrinking the size.   This common engineering challenge can bump up your processing needs from a simple, low cost microcon ...

Filter Blog

By date: By tag: