• Embedded Vision Quiz

    Embedded Vision Quiz sponsored by       Quiz | Xilinx | On Semiconductor | Sensors | Embedded   Combining embedded systems with computer vision results in Embedded Vision Systems. But h...
    Profile Photo
    last modified by pchan
  • TinyML combines machine and deep learning models on tiny hardware

    The Arduino Nano 33 BLE Sense. (Image Credit: Arduino)   Developing machine learning (ML) algorithms for hardware involves complex mathematical models based on training data. Using this approach enabled it to ma...
    Profile Photo
    last modified by Cabe Atwell
  • Is it just me or is there really a global stock shortage or supply issue with components and modules

    I've been aiming to replenish and order in some new components for various projects and couldn't help notice how many popular components are out of stock and awaiting delivery. It just appears to be worse than usual. ...
    Profile Photo
    last modified by BigG
  • AWS IoT: convert a character array into JSON in a MQTT Rule

    This is a little side note, related to the project Arduino Day Workshop: NanoDrone II: AI and Computer Vision with LoRa (Win a PSoC6 and a Pair of MKR 1300 Boards!). In this project, 4 attributes are sent to Amazon W...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6 and ModusToolbox: UART receiver with FreeRTOS - Deep Sleep support

    The steps to integrate incoming UART data with FreeRTOS on a PSoC 6. Part 2: now with low power support.   image source: Infineon application note AN219528 PSoC 6 MCU Low-Power Modes and Power Reduction Tech...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6 and ModusToolbox: FreeRTOS message queue

    The steps to use an RTOS message queue to exchange data between tasks. In this post, we post data from the low level hardware (UART peripheral) to a task that handles a logic part of our firmware.   This is ...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6 and ModusToolbox: UART receiver with FreeRTOS

    The steps to integrate incoming UART data with FreeRTOS on a PSoC 6. The focus is on saving processor power. The design does not poll for incoming data. It yields all powers to the RTOS scheduler (possibly going to ...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6 and ModusToolbox: Create a FreeRTOS 10.3 Project

    The steps to create an empty PSoC 6 project and run FreeRTOS on the CM4 core.   It's easy to set up a FreeRTOS project in ModusToolbox. The simplest way is to start from one of the examples of the IDE's Applic...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6: Low Power Management - Power consumption without WiFi or Bluetooth

    When you're making a low power design, it's interesting to know the energy use of your gizmo. In this 2nd post of the series, I measure the current in the different power modes. image source: readme file of the PS...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6 and ModusToolbox: Create a Project with its own Board- and Module configurations

    By default, projects in a workspace in the Cypress ModusToolbox IDE (mtb) share board and device configuration files. There are several good reasons to do this, but it's not always what you need. If you want to buil...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6 and ModusToolbox: Break the Debugger from the Proto Board

    In this post: what happens if you remove the debugger. Will everything still work? What's the difference?   TL;DR: you can still use all functionality.   Difference when debugger is broken off  Wh...
    Profile Photo
    last modified by Jan Cumps
  • PSoC 6 and ModusToolbox: FreeRTOS to AWS MQTT

    In this post we react on a message on the RTOS queue and publish its payload on Amazon's AWS IoT MQTT service.   Together with the two previous posts, this one describes a hardware component in the NanoDrone...
    Profile Photo
    last modified by Jan Cumps
  • Embedded Vision Quiz Resource

    Embedded Vision Quiz Resource sponsored by       Quiz Resource | Xilinx | On Semiconductor | Sensors | Embedded | Return to Quiz   Question 1: Embedded Vision Versus Machine Vision: What's...
    Profile Photo
    last modified by pchan
  • What can you do with a GHz MCU?

    Despite the thousands of development boards that have shipped and the overwhelming interest from the market for the i.MX RT1170 crossover MCU, I do come across an occasional customer that does not understand the value...
    Profile Photo
    last modified by kjachim
  • Ardurino intelligent irrigation solution.pdf

    1 Product function: it is used to realize intelligent irrigation of green plants, orchards and so on, and ensure that the soil humidity of plants is maintained in the range suitable for plant growth. (1)Real time de...
    Profile Photo
    last modified by aa19989291995
  • Create a cloud based noise pollution monitor using Digital Discovery

    Noise pollution directly affects the quality of life and health. With Digilent Pmod MIC3  and Digital Discovery, you can create a cloud-based noise pollution monitor to assess the noise impact.   The Pmod M...
    Profile Photo
    created by alexwonglik1
  • how do i access RAM on a USB flash drive ?

    hello smart people, nerds, wiz-kids and enthusiasts   i need the protocol to access memory on a USB stick   i know that i send address, data and control information to access a location in flash ram, but...
    Profile Photo
    last modified by TaylorTronics
  • Getting Started with the USRP B205mini-i software defined radio platform

      The USRP B205mini-i is a flexible and compact platform that is ideal for both hobbyist and OEM applications. It is designed by Ettus Research™ and provides a wide frequency range (70 MHz to 6 GHz) and a ...
    Profile Photo
    last modified by alexwonglik1
  • 4 LED control using capsense PSoC 4

    Dear all, I'm using cy8c4245axi-483 MCU to control 4 LED with capsense module. Here I have attached code and problem Statement. In this code if we touch 3 times up button and 3 times down button then it is working fi...
    Profile Photo
    last modified by premkb
  • Doesn't work properly

    Open video

    Profile Photo
    last modified by premkb