Skip navigation
The DSP48 Primitive - Inferring larger multipliers   The DSP48E2 primitive contains a signed 27x18 multiplier, any signed multiplier up to this size can be implemented with just one such primitive. If we need larger multipliers we can achieve that with multiple DSP48s.   The way larger multipliers are built uses a feature of the DSP48 primitive in which the 48-bit dedicated P cascade output of one DSP48 is right shifted by 17 bits before being added to the partial product calculate ...
The DSP48 Primitive - Small Multiplications - Two For the Price of One   The DSP48E2 primitive contains a signed 27x18 multiplier, any signed multiplier up to this size can be implemented with just one such primitive. Unsigned multiplications are of course possible if you add a zero MSB bit to the operands and then treat them as signed but the largest unsigned multiplication that can be done that way with one DSP48E2 is 26x17.   When the operands are much smaller it becomes possib ...
From: https://thetinysynth.wordpress.com/ The Tiny Synth, with its synthesis core measuring only 1.5×1.5mm, is probably the smallest subtractive synthesizer out there. Based on the Artix7 device from the latest Xilinx FPGA family, it provides a total of seven oscillators, three LFOs (Low-Frequency Oscillators), two envelope generators, tremolo and vibrato effects and an SVF (Static Variable Filter) with resonance and frequency control. The Artix7 device, the core of The Tiny Synth.   ...
The DSP48 Primitive - Wide XOR Mode   The DSP48 primitive can be used for more than just multiply and accumulate. It can for example implement very wide XOR functions. Apart from the obvious ability of XORing two 48-bit operands using the A concatenated with B, or A:B and C inputs and producing a 48-bit result on the P output, or 48 XOR2 logic functions, it is also possible to implement 8 XOR12s, or 4 XOR24s, or 2 XOR48s or one XOR96 with a single DSP48E2. It is also possible to compute a ...
The DSP48 Primitive - Symmetric FIR with DSP48 Primitive Instantiations   We will now add the option of choosing between DSP48 inference or primitive instantiations to the symmetric FIR introduced in Post 22. It might make sense to review Post 22 and Post 23 before continuing.   We will use the same technique, the generic BEHAVIORAL can be set to TRUE or FALSE to select between the two implementations. This is very similar to the code used in Post 24, except that now we are using the ...

Filter Blog

By date: By tag: