Skip navigation
A key feature of Avnet's Ultra96-V2 board is its WiFi and Bluetooth connectivity that is made possible using the on-board ATWILC3000 module from Microchip. This module is IEEE 802.11 b/g
plus Bluetooth 5 LE and is certified in more than 75 countries globally.  The module provides SDIO (WiFi) and UART (Bluetooth) interfaces for connecting to the host processor and can achieve WiFi throughput of up to 46 Mbps UDP & 28 Mbps TCP/IP.  Though this is a very popular module that is used ...
The Xilinx Zynq UltraScale+ MPSoC device has an integrated Platform Management Unit or PMU. This PMU's functionality is described in Chapter 6 of Xilinx UG1085, Zynq UltraScale+ Device Technical Reference Manual. The PMU controls many things on the ZU+ device, including powering up and down the ZU+. The Ultra96-V2 incorporates an On/Off controller to interface between the on-board power regulators and the ZU+. This allows the ZU+, Power Button, and regulators to seamlessly work together to power ...
I wanted to create a quick post explaining a small trick I noticed in the build process that allowed me to efficiently complete a build for Vitis and the Xilinx ZCU104 development platform.  I learned that if you abuse a tool, you can still make it behave improperly!   Summary: Uncheck the Autoupdate checkbox during an Ubuntu 18.04.1 LTS install Make sure to check that the # of JOBS being called out does NOT exceed the # of cores assigned to your Virtual Machine   Details: I ...

Filter Blog

By date: By tag: