Skip navigation
Hi all,   I've seen quite a few recent posts with people seeing USB 2.0 speeds / connectivity when using the MPSoC.  I wanted to let you know that after scouring the interwebz, I think I've pooled enough information together to try to help you with your issues. If you are already familiar with USB 3.0 and transceivers, you can skip to the end!  Or stick around, you might learn a thing or two!   As USB speeds have risen from the lowly 1.5Mbps to the great 5 Gbps that we see ...
Avnet has partnered with Adam Taylor to offer three FREE days of training to help you get started with Xilinx Embedded Design! These trainings include a mix of recorded lectures and hands-on labs with the Avnet MiniZed Development Board. The trainings are targeted at new users, so if you've wondered where to begin, this is the place!     The trainings are based on the Xilinx 2019.1 tools. We are aware that 2019.2 is now out, including Vitis. Hopefully we will update the trainings in ...
Introduction This project is a follow up from the previous project on porting the PYNQ framework to the ZC702 development board. In this article we will show how to leverage the xOpenCV framework in conjunction with the PYNQ framework  to implement a basic image processing pipeline on ZYNQ series FPGA SoC . The project will be developed on a ZC702 development board using a generic USB camera.   Now , we will look at developing an end to end system for resizing live video using the ...

Filter Blog

By date: By tag: