We have now released the 2020.1 BSP for both Ultra96-V2 and UltraZed EV with the PMIC programming utility built in! For the purposes of this blog, I am going to provide instruction on how to simply download the 2020.1 BSP as an SDcard image. You will then need to use a program such as Etcher to create the SDcard from the image. First download the appropriate image here - http://avnet.me/zedsupport Click on the 2020.1 folder, then go to the Vitis_PreBuilt_Example folder. From here select ...
As a follow up to the blog I posted on building the hardware design for the out of box image for the ON Semiconductor Dual Camera Mezzanine card, here are the instructions to complete the build with the Petalinux project. The original blog can be found here - Ultra96-V2 ON Semiconductor Dual Camera Mezzanine hardware build instructions The process of porting the full design over to our Github repo has now been completed. Below I've pasted the instructions to build the full design includ ...
I'm going to borrow heavily from my colleague Tom Curran and his excellent HDL howto blog (Avnet HDL git HOWTO). I highly recommend reading through that blog before continuing. I will modify it as needed to help you build the hardware design for the 96Boards ON Semiconductor Dual Camera Mezzanine design using Ultra96-V2. I will preface this blog post by saying I have been a power and hardware designer most of my career. In an effort to diversify and help out on more projects I've decided to lear ...