Skip navigation

FPGA Group

4 Posts authored by: rscasny element14 Team
I had a lot of interest in my giveaway for the Digilent CMOD S7 board, so I am offering another giveaway for 2 members who are interested in experimenting with a Spartan-6 FPGA. Let me tell you about the board first.   It's called the Cmod S6 -- a Breadboardable Spartan-6 FPGA Module.   It's small, featuring a 48-pin DIP form factor board built around a Xilinx Spartan 6 LX4 FPGA.   The board also includes a programming ROM, clock source, USB programming and data transfer circ ...
Introduction They may seem like an unlikely or odd couple: art and technology. Art implies the vast realm of unbridled creativity, while technology is bounded by empiricism: rules, standards and rationality. But when art and technology are interwoven, new vistas are revealed, new ideas are born, and new technologies with a distinctive twist are realized. In his Art of FPGA Design Series, Xilinx employee and designer Catalin Baetoniu breathes life into the finer points of designing with FPGAs. E ...
A Field Programmable Gate Array or FPGA is an integrated circuit that could contain millions of logic gates that can be electrically configured to perform a certain task. But how does an FPGA compare to a microcontroller, microprocessor or an application specific IC?.   Microcontroller vs FPGA: The structure of a microcontroller is comparable to a simple computer placed in a single chip with all of the necessary components like memory and timers embedded inside. It is programmed to do some ...
Field-programmable gate arrays (FPGAs) are reprogrammable silicon chips. They can be programmed for different algorithms after fabrication. Modern FPGAs consist of up to millions of logic cells that can be configured to implement a variety of software algorithms. Although the traditional FPGA design flow is more similar to a regular IC than a processor, an FPGA provides significant cost advantages in comparison to an IC development effort and offers the same level of performance in most cases. & ...

Filter Blog

By date: By tag: