Skip navigation

Industrial

11 posts
One of the biggest cybersecurity issues facing the world today is the venerability of the so-called Internet of Things. Every day millions of unsecured IoT devices are utilized in DDOS attacks by hackers, bad state actors, and botnets. This is one of the reasons that the Raspberry Pi Foundation decided to turn off SSH access in Raspbian by default just a few years ago, but now with more and more devices joining the IoT every day, something has to be done on a larger level to prevent cyberattacks ...
This post entry provides a detailed description of how the Device-to-device communication demo was developed so that you can leverage this knowledge to integrate NFC into your own system. This document has been structured as follows:     Introduction Device-to-device communication demo functionalityNFC for communication with a batteryless unit NFC for communication between two devices mounted in close proximity NFC for communication with a rotating part as a cable replacement solut ...
(Image credit: University of Bristol via YouTube)   As strange as it may sound (literally), we could one day float in midair with the help of sound waves. A little technique known as sonic levitation. Engineers from the University of Bristol have created a new acoustic trap that produces two vortex-shaped sound waves to trap (levitate) objects more massive than the wavelengths themselves.   According to the engineers, “This discovery opens the door to the manipulation of drug c ...
The research team at MIT are using oxide materials, like those found in rechargeable batteries, to create actuators that bend and perform in high heat. This actuator shouldn’t cave in under pressure (Photo via MIT)   It’s not exactly easy to carry out maintenance tasks inside a nuclear plant. Equipment doesn’t always hold up and breaks under pressure. The Tokyo Electric Power Co. learned this the hard way when they sent in a robot inside Fukushima’s nuclear reactor, ...
The Department of Transportation has released guidelines concerning the safety of automated vehicles. Olli, a 3D printed self-driving trolley pictured above, made its debut at the International Manufacturing Show this September in Chicago. (via amtonline)   As with much new technology there are flaws, which must be addressed before the product is mass marketed. After the self-driving car made by Tesla fatally crashed this past May, it was clear that we were a ways away from seeing roads s ...
Comma One is part of George Hotz's startup Comma.ai and only works with a small number of cars. Comma One works with its camera and your car's radar (Image via Comma.ai)   Like 3D Printing and VR/AR... the autonomous, self-driving, car is the new hot thing to get in on. One company did just that. Is there room for more?   With new automated features like self-parking and self-start up being introduced to cars every year, it's only a matter of time before they start driving themselves ...
As an NDT equipment manufacturer, you’re looking to gain that competitive advantage with precise measurements that are cost effective.   How can we help? By providing high performance, standard and focused transducers built from specialized ceramics that:   easily integrate into your handheld detectors survive in harsh conditions of a permanent installation reliably operate in immersed conditions Why choose us? Your NDT products need ultrasonic solutions that are built to w ...
What is UL 508A? UL 508A is the UL standard for the construction of Industrial Control Panels. This blog gives guidelines to panel builders on various issues including proper component selection, wiring methods and calculation of short circuit current ratings. If a customer follows UL’s recommendations, they can apply to have their panel listed by UL. Upon successful inspection, the panel would bear the UL label. It is important to ask your customer if they are building to this standard, ...
What is UL Standard 508A? UL508A is the UL standard for the construction of Industrial Control Panels. This document gives guidelines to panel builders on various issues including proper component selection, wiring methods and calculation of short circuit current ratings. If a customer follows UL508A’s construction requirements and recommendations, they can apply to have their panel listed by UL. Upon successful inspection, the panel would bear the UL label. What is the impact of NEC 2005 ...
  Gangnam Style by PSY took over silicon valley. Inspiring, exciting, and devouring the time of those at the forefront of technology. In fact the valley company "Viki" has taken it upon themselves to translate the video into 17 languages (part of what their company already does in town). A month ago it took over the offices of every one of my engineering associates. I'll admit, I've played it more than once.   Sometime music drive us to create. Maybe it will for you too.     ...
I am creating a development blog following the dicussion here: Let's Design 2 : The LED shake light The idea is to showcase the process of collaboration and design in an easy to follow series. From the original post: I want to make a  device that, when it is shook, it will turn on a LED. Shook again, and  it turns off the LED. I would like to add other features, like varying  light patterns, but let's address the base issue of turning on one  light.   The req ...

Filter Blog

By date: By tag: