Skip navigation
shabaz

Cisco Live 2017 in Berlin

Posted by shabaz Top Member Feb 24, 2017
The week-long Cisco Live finished today, and due to work I had extremely little time this year to check out the exhibits. I think I spent ten minutes before it closed : ( Anyway, here are the brief snippets that were possible to capture in ten minutes!   Firstly, a quad-Pi train : )   Every year the train demonstrations seem to get better. This years model looks very slick. End-on view. The small rectangular white and black thing inside near the front is some Bosch gadget: &# ...
A new development between IBM and Arrow Electronics lets IndieGoGo Developers use Watson’s cloud services and tools. IBM is slowly bringing Watson to the masses. (via IBM)   IBM’s Watson is best known for beating Jeopardy champ Ken Jennings in 2011 and lately, you may have seen its name pop up in H & R Block ads. Now, IBM is ready to share Watson with the masses. At the unveiling of the company’s $200 million Internet of Things headquarters in Munich, they also reveal ...
Over the past decade, the popularity of Python as a mainstream programming language has exploded. Notable advantages of Python over other languages include, but are not limited to; It is a very simple language to learn and easy to implement and deploy, so you don't need to spend a lot of time learning lots of formatting standards and compiling options. It is portable, expandable and embeddable, so, it is not system dependent, and hence supports a lot of single board computers on the market the ...
      The IoT paradigm has brought with it a decided change in a number of areas ranging from hardware design to services offered by software companies. One of the aspects most affected by this is that of Communication Protocols.   A communication protocol can be thought of as a language that is used by two or more machines to talk to each other. It is a set of rules that are followed by the two devices in order to make sense out of the messages that they pass to each ot ...

Filter Blog

By date: By tag: