Skip navigation

Internet of Things

4 Posts authored by: doctorcdf
  At the Consumer Electronics Show in January 2014, John Chambers, CEO of Cisco, said that the IoT would lead to greater efficiency, better decision making and contribute over 19 trillion dollars to the global economy.At element14, we were already ahead of the curve.  Our first webinar referencing the Internet of Things occurred in 2012. In late 2013, we launched the "Smarter Life" design competition, whose main emphasis was to advance the development of smarter, networked appliances. ...
doctorcdf

IoT Lives!

Posted by doctorcdf Nov 17, 2014
There has been a bit of chatter this week that the Internet of Things, or at least the three letter acronym IoT...is dead. Indeed our friends at Electronics Weekly wrote a comment piece this week "IoT RIP" which kind of suggests it might be. Now I don't want to upset anyone but when I was at Electronica, I saw no indication that the days of the IoT acronym were numbered. On the contrary, it was all IoT all the time. I did see evidence that the technology is moving from the "hype" phase to the ma ...
Internet of [der] Thing(s) [Dinge] Nomen Ein globales Computernetzwerk, das eine Vielzahl an Informationen und Kommunikationsmöglichkeiten bietet. Es besteht aus miteinander verbundenen Netzwerken, die standardisierte Kommunikationsprotokolle verwenden. Präposition Steht u.a. nach einer Zahl, einem Zahlwort oder einer substantivischen Bezeichnung des geteilten Ganzen als Kopf der Phrase. Nomen Ein Objekt, dem man keinen bestimmten Namen geben muss, kann oder will. Ich nehme diese F ...
Click here to view the webinar video. Q: Do you think a separate low power network across cities are required, or the existing GSM/3G/4G networks can be used to enable wider use of IoT? No I don't think so. I think it is partially required in some cases but in general no. The reason is that wifi networks are widely available. As such, we can utilize existing infrastructure. In case isolated locations are required or very long range, there are technologies that can enable long range (such as sub ...

Filter Blog

By date: By tag: