Skip navigation

Internet of Things

8 Posts authored by: main8096
WIZnet has been registered and listed as a platform partner on ARM® mbed™ developer site.     The ARM® mbed™ IoT Device Platform simplifies and speeds up the creation and deployment of commercial, standards-based Internet of Things (IoT) products at scale by building a new operating system, software components, tools and ecosystem that will make this vision a reality.        -   For more information, https://developer.mbed.org/ ...
  Dears.   WIZnet make a better Inspiring Smart & Cost-effective one chip solution which integrates Cortex-M0 and Hardwired TCP/IP core for various embedded application platform especially internet of things.           <for more information: http://wizwiki.net/wiki/doku.php?id=products:w7500:start>       In the IoT application space, Sensor Nodes are enabled by a number of fundamental technologies, Connectivity Internet, and strong ...
main8096

WIZ550io Internet Radio

Posted by main8096 Dec 10, 2014
Let’s start the Internet radio project with WIZ550io Please refer to YouTube 1. Block Diagram (main interface) -       SPI1: WIZ550io  -       SPI2: VS1033D -       Define the VS1033D pin -       Define the WIZ550io pin 2. Schematic & Source code & Compiler - Refer to as below site https://www.dropbox.com/sh/ok ...
Xively Demo with WizFi250   Let me introduce the “Xively server and WizFi250 application note.   In order to Test, the customer should make a Xively ID and acquire Channel and API key.   (For more information about the Xively, Please check the Youtube or Google)       This test environment is as below   •Feed ID : 1805123826   •X-ApiKey : H3lr9T1As7ADOfpXCvg8fdcUYC3wX39tXVUBGAIKvouibJnM   •Channel : Demo     & ...
  Google Developers Console(Project Management, API Key, Project ID) https://console.developers.google.com/                                     GCM Sender(Android App for GCM test) https://play.google.com/store/apps/details?id=com.eastandroid.gcmsender   Raw Data File to send to GCM Server (738 Byte) ? 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 POST /gcm/send HTTP/1.1 Host: android ...
The WizFi250 EVB is the evaluation board for testing WizFi250 and prototyping development. WizFi250 EVB is composed of a WizFi250 evaluation board and a WizFi250 module.     Feature Identification Button Description   WizFi250 Reset Through this button, user can restart WizFi250 module. Function Through the function button, user can enter specific mode without AT Command. ♦ Factory Recovery : When doing Boot or Reset, press the button over 3.5 seconds ♦ ...
WizFi250 offers a quick, easy, and cost-effective way for device and appliance manufacturers to add WiFi capabilities to their products. WizFi250 provides UART and SPI interfaces which enable connections to any embedded design utilizing an 8/16/32-bit microcontroller via simple AT commands. WizFi250 is an ideal solution for organizations with limited or no WiFi or RF expertise, as it not only reduces RF design time but also removes the burden of testing and certification, allowing customers; ...
The earlier W5100 and W5200 chips achieved success by bringing the benefits of hardware TCP/IP protocol processing to low-cost applications.  The W5500 carries forward all the major features of the earlier chips; - Full featured 10/100 Ethernet MAC & PHY - Hardware TCP/IP Protocol Processing - 8 independent sockets - 32KB RAM buffer   New W5500-specific enhancements include a faster and more versatile SPI interface (up to 80 MHz) and ability for the host MCU to flexibly ut ...

Filter Blog

By date: By tag: