Skip navigation
1 2 Previous

Internet of Things

18 Posts authored by: mubeen.abbas
OverviewDesigning your own POS terminal can be a demanding task and getting the product certified often reveals the next big challenge. With the PN5180 NFC frontend, NXP eases the design process paving the way for EMVCoL1 contactless certification. Furthermore, with features such as Dynamic Power Control (DPC) or Adaptive Receiver Control (ARC), the PN5180 helps overcome tough requirements that come with payment specifications. This significantly helps the customers to reduce their time to marke ...
Audio speakers and headphones are becoming wireless, with Bluetooth and Wi-Fi as the most popular technologies. NFC is the fast and simple way to associate wireless devices, without creating conflicts. No menus, no waiting. The most advanced solution for NFC pairing is connecting two Bluetooth enabled audio devices with just a tap, which creates a multi speaker audio system, or even a ‘silent disco’ if you use two headphones. In the webinar (link below), you will learn how you can ...
In the previous blog of January 2020, we learnt how to integrate NFC controllers in Linux and also how NFC frontend offers a host interface and a contactless interface.   This blog is the extension of previous two sessions and here we will talk on how to port the NFC Reader Library to K64F.   In this session, using a real porting example, we show the steps required to port the NFC Reader Library to a target MCU.   The goal of the session, is to serve as a guide for software develo ...
If you are a software developer and want to integrate an NFC reader into your device, this webinar demonstrates the procedure. NFC frontend offers a host interface and a contactless interface. Host interface is a low level access to the contactless interface providing full access to the IP. The host controller uses the register access to the contactless interface : to configure RF framing and signaling. to finally transfer the RF digital protocol based blocks to/from a counterpart. An NFC fr ...
The NFC antenna design is one major part in every NFC reader design. For a proper NFC reader design, it is required to have the insights and skills about choosing the right antenna for your purpose as well as knowing the NFC antenna tuning procedure.   The important considerations to take into account from the NFC reader design perspective apply at the component level.   From the reader IC perspective, we need to consider: ·        The RF prot ...
  Today, the growing number of NFC smartphones enables intuitive interaction with just a tap to your smart device. Take the Smart Home example: very often complexity comes with the first setup of devices that are as diverse as the standards under which they operate. NFC provides simplicity in the entire home network. With just a tap, new objects and devices are easily connected to the network. NFC is perfectly complementary with the other wireless technologies whether it's ZigBee, WiFi, Blu ...
The Internet of Things or IoT is a buzzword these days.   Generally speaking, IoT refers to all kind of objects…. from medical equipment, appliances, wearables, meters, to cars….  which get equipped with sensors and network capabilities so they are able to collect and exchange data.   The Internet of Things does not refer to any specific technology, but actually, it is made of many technologies working together in the direction to…. increase automation, safe ...
The CLRC663 plus is the follow-up to the groundbreaking CLRC663. It delivers optimal performance in every application and offers a special low-power support to make battery-powered systems more efficient.   CLRC663 plus is ideal for a wide range of applications, including access control, payment, gaming and industrial. It’s an excellent choice for any design with high performance requirements. If you need the best NFC performance or the lowest power consumption, CLRC663 plus is your ...
Homes are increasingly connected. Everyday appliances, from lights and ceiling fans to washing machines are now being connected to the Internet. Consumers will be able to control appliances, monitor and manage energy consumption, increase comfort and enhance entertainment to a whole new level as NFC enabled consumables make the Internet of Things (IoT) a reality. Our mobile device will increasingly become the ‘remote control for our lives’. Connecting our appliances to the home netwo ...
NFC adds the magic to gaming. Incorporating NFC tags into games and toys allows for an interactive connection between the physical and virtual worlds. NFC can enhance the experience with any kind of toy or game, from classical board games that interact with NFC-enabled devices, to trade cards and figurines that come alive in the virtual world when tapped against smartphones or consoles, to smart toys communicating with each other. In all of these use cases NFC enhances the gaming experience and ...
With Apple’s recent launch of iOS12 and the iphone XS and XR, NFC just got another big boost. Now almost two billion people worldwide who own smartphones will also have an NFC reader to interact with NFC tags. Join the exciting world of NFC with its limitless possibilities that deliver great user experience whilst enabling new value-driving industrial, medical and consumer applications.   Please see attached webinar recording and slides for further details. ...
Get the latest updates on the NXP portfolio for payments and discover the existing POS Reader solution kit (SLN-POS-RDR) as well as all the available support tools. ...
NFC is a great way to identify and authenticate consumables & accessories in industrial and consumer products. Using NFC helps to ensure that only genuine parts are being used and allows to make adjustments of device settings according to part manufacturer, type and end user preferences. See attached slides for further details. ...
This post entry provides a detailed description of how to develop an NFC pairing solution for audio devices. For that, we will describe in detail an audio speaker prototype made by NXP. This post entry has been structured as follows:     Use cases for Bluetooth and Wi-Fi pairing via NFC Benefits offered by the NFC pairing solution Pair and unpair Bluetooth headsets with just a tap with NFCNFC pairing process steps NFC unpairing process steps Multi-audio wireless speaker demo with ...
Here is a detailed explanation of the most exciting, out of the box and interesting demo for NFC made by NXP. It is called "NFC Cube".     NFC cube is an interactive demo which anyone would love to have on their desk whether working with NFC technology or not. For the geeks and engineers fond of technologies this could be a great activity to build something like this for themselves as a hobby. You can get the NFC parts that are easily available in the market. Moreover all the design ...

Filter Blog

By date: By tag: