Skip navigation

Internet of Things

2 Posts authored by: satyavrat
Over the past decade, the popularity of Python as a mainstream programming language has exploded. Notable advantages of Python over other languages include, but are not limited to; It is a very simple language to learn and easy to implement and deploy, so you don't need to spend a lot of time learning lots of formatting standards and compiling options. It is portable, expandable and embeddable, so, it is not system dependent, and hence supports a lot of single board computers on the market the ...
      The IoT paradigm has brought with it a decided change in a number of areas ranging from hardware design to services offered by software companies. One of the aspects most affected by this is that of Communication Protocols.   A communication protocol can be thought of as a language that is used by two or more machines to talk to each other. It is a set of rules that are followed by the two devices in order to make sense out of the messages that they pass to each ot ...

Filter Blog

By date: By tag: