Skip navigation
1 2 Previous

Moto Mods

24 posts
jimmy6472

Moto test phone

Posted by jimmy6472 Feb 17, 2019
Hi Im am in Australia, this is not Austria, we are 10-20 years behind Europe in all things tech, I use  a chinese phone to test all my circuits on the job, a Senter 327(China Shandong), its a PDA, a smart phone with  additional features, can be a Volt Ohm Meter,  can test for smart TV traffic, can test for ADSLxyz, can send red light on optical port, can measure optical on auxiliary optical port, can make POTS phone call, using keypad, is a smart phone 3G, runs android, bar code ...
  In 2016 MotoMods and Indiegogo launched "Transform the SmartPhone 2016" contest, in which Motorola and Indiegogo helped you to create a custom, snap on, add on for the Motorola Z family of phones.   Current Mods include Amazon Alexa Speaker set, a Projector, a high end camera, Sound Boost speaker set, wireless charging or just a supersized battery pack.   Build The Unexpected Can you create a moto mod that helps people discover new ways to connect, work and entertain?  ...
  Perforated Board   At a glance the perforated board seems like a nice expansion board. It looks like you can solder your projects directly to the board, plug it into the back of your phone, and away you go with a new custom feature you added to your phone. From the look of the board, most developers would say “oh that looks convenient to get my own custom electronics interacting with an app on my phone.” But, they’re completely wrong.   The board has 26 rows ...
I have a Moto-Z and need to include the LAN9500A driver in the linux kernel since my USB device uses that chip.  Is there instructions on how to build a Android ROM for the Moto-Z that would include this driver?   Thx, Y- ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
See part 8 here.   Before we compile Nuttx, we need to change the hardware manifest file. The .mnfs file for Blinky is located in .
uttx/apps/greybus-utils/manifests as created above.     Add the following lines to the end of the document:     At the top of the file we can input a string that will show on the app when the firmware is loaded. In [string-descriptor 2], I named my firmware “MDK-RAWBLINKY”     Cabe http://twitter.com/Cabe_e14 ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...
Index of the Moto Mods Developer project: Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install Moto Mods Developer Part 3 - Firmware Setup Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard Moto Mods Deve ...