Index of the Moto Mods Developer project:

Moto Mods Developer Part 1 - Getting Started - Virtual Machine Setup and Linux Install

Moto Mods Developer Part 2 - Getting Started - SDK Setup & Android Studio Install

Moto Mods Developer Part 3 - Firmware Setup

Moto Mods Developer Part 4 - Getting Started - Make Build-Folder, add Utility and OS files

Moto Mods Developer Part 5 - Flashing Firmware with MDK Utility

Moto Mods Developer Part 6 - Blinking an LED on the Moto Mods Perfboard

Moto Mods Developer Part 7 - Modifying the C file for the perfboard LED

Moto Mods Developer Part 8 - Configure Nuttx

Moto Mods Developer Part 9 - Updating the Hardware Manifests file

Moto Mods Developer Part 10 - Cont’d Configure and Compile Nuttx

Moto Mods Developer Part 11 - Load newly created Nuttx Firmware onto Reference Board

Moto Mods Developer Part 12 - Soldering the Test Points to use the perfboard

Moto Mods Developer Part 13 - Making custom App to control the Firmware

 

 

{gallery:autoplay=false} MotoMods Developer Part 10

1.png

Step 1:Now that we’ve edited the Hardware Manifest file we need to go back and configure it back in menuconfig

2.png

Step 2:Scroll down on main menu

3.png

Step 2:

4.png

Step 2:

5.png

Step 3: Click on the last field, we will name this field the same name as the Hardware Manifests file “hdk-blinky.mnfs”

6.pngR

 

Step 4: Exit 3X.

7.png

Step 5: Configure the Bootloader

8.png

Step 6: Compile Nuttx

9.png

Step 6:

 

 

The above gallery is also the pictures and text below:

 

Now that we’ve edited the Hardware Manifest file we need to go back and configure it back in menuconfig

1.png

$ cd $BUILD_TOP/nuttx/nuttx

$ make menuconfig

 

Application Configuration  --->

  -*- Greybus utility  --->
    Select a predefined Manifest (Custom manifest)      
      (hdk-blinky) manifest name

 

Scroll down on main menu

 

 

 

 

Click on the last field, we will name this field the same name as the Hardware Manifests file “hdk-blinky.mnfs”

Enter “hdk-blinky”

 

 

Hit Ok and scroll right and press Save.

 

 

Exit 3X.

Configure the Bootloader

 

7.png

 

Compile Nuttx