Skip navigation
Physicists from MIT create a new material that produces a record amount of energy under a strong magnetic field. MIT finds a way to significantly boost thermoelectricity’s potential. (Image via MIT)   We’re constantly looking for ways to make energy self-sufficient and more eco-friendly. One possible method is using the heat generated from certain objects to create energy. For instance, the heat generated from your car engine could help power your car. This is possible if impro ...
University of Arkansas researchers have shown that the motion of graphene could supply an unlimited amount of clean energy. (Image credit: Pixabay)   Graphene advancements are rolling out on a regular basis, with new developments in production, strength, and have even used it to create 3D printed objects. Researchers from the University of Arkansas have also utilized the material to create a source of potential unlimited clean energy, thanks to its flexibility.   Professor Paul Thibad ...
A new membrane technology uses a process to extract hydrogen from ammonia to fuel cars. The CSIRO team hard at work on the membrane technology. (Photo via CSIRO)   In the never-ending quest to create fuel-efficient and eco-friendly cars, hydrogen fuel seems like a great option. Unfortunately, it presents a whole mess of problems, like being highly flammable, figuring how to store it, and being difficult to ship due to its low density. These issues prevent hydrogen from being progressed as ...

Filter Blog

By date: By tag: