Stanford University consistently brings us innovation. It’s astounding. An example of that is the team of engineers who created a clever way to transmit electricity wirelessly. The technology could send electricity to moving electric cars, drones and robots, and could be applied to electric cars driving on the highway or drones flying in the sky after it is scaled up.

 

Although a revolutionary idea, wireless electricity is a project, the team had been working on for a while now. Shanhui Fan and Sid Assawaworrarit, the two researchers working on the project, confessed that the initial prototype was not reliable enough to be used outside the lab. About three years ago, the researchers developed a charging tool that could charge a receiver even when the distance to the latter fluctuated. The feat was possible thanks to the combination of an amplifier and a feedback resistor, which permitted adjustments to the operating frequency despite the constant change in distance. Unfortunately, the system could only transmit ten percent of the power it generated, output, which has now been improved.

 

For the new version of the system, the researchers replaced the original amplifier with a “switch mode” amplifier, which allowed the system to transmit more than 90 percent of the electricity flowing through it. With this improvement, the researchers would be able to transmit about 10W of electricity to a receiver as far as 3 feet away. Fan and Assawaworrarit are confident that it will not take much more to bring the system to the level where it transmits hundreds of kilowatts to an electric car. According to their calculations, it will be possible to charge a car going at 70 miles per hour in a fast manner if it goes through a charging area of approximately 4 feet.

 

We are talking about a super-fast charging on the fly, which brings up the questions of whether the battery of the electric cars on the market can absorb electricity that fast. Super caps? I’m not at all certain that much intense energy blasted at people constantly would be safe despite the researchers assure us that their technology presents no risk for the human body.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell