When you think of a company or home that is powered by solar energy, it's quite likely that you immediately think of solar panels. These highly visible, integral pieces of equipment usually get all the credit. But there are a number of other devices within a solar energy system—such as the solar inverter—that are key to its functionality. This post was inspired by the Solar Inverter Dev Kit I stumbled across. Image Credit: Solar Inverter Dev Kit ...
These lines show the temperature a sample must reach (10 kelvins) to exhibit superconducting behavior. (Image Credit: 2020 Okazaki et al.) Superconductors, a material that allows electricity to flow through it with absolutely no resistance, could be very beneficial for future electronics. For the first time, researchers from the University of Tokyo in Japan found a way to create a superconductor from Bose-Einstein Condensate (BEC). The commonly known states of matter are solids, ...
Posted by
ngi Nov 12, 2020
The durability test system for high-voltage electrical appliances is designed by NGI for the endurance & reliability test of electrical components such as fuse boxes in automobiles, rail transit, household appliances, aircraft, ships, medical equipment and other related products. Diagram of durability test system (This diagram is only for refer ...
This all-electric school bus only has a 135-mile range, which is more than enough to transport students to school in Tok, Alaska. (Image Credit: KTUU) It may look ordinary, but it’s actually Alaska’s very first all-electric school bus. Soon enough, it will be used to transport students in Tok, Alaska, to school. Constructed by Thomas Built Buses in North Carolina, the Jouley bus was purchased by Tok’s transportation service with the help of an Alaskan Energy Authority g ...
The role of battery simulator is to emulate various output states and charging & discharging characteristics of real batteries. It can change the battery SOC, depth of discharge, open circuit voltage, internal resistance and other conditions at any time according to the needs of users, and rapidly verify the DUT's response under different battery conditions. In short, it is a virtual battery to replace real batteries to execute various test. Nowadays, most consumer electronics need ...