Skip navigation
This blog continues from my original review here  RoadTest the Keysight U1282A Digital Multimeter - Review       Following some testing using an Android Tablet and Bluetooth connection, I thought I'd see what the PC software offers.   Keysight Handheld Meter Logger ver_3_1_51130_01 While the Android version downloads and installs and just works, the PC version has a few issues.   1.     The install gives you (the PC Owner) no control over where ...
This is my first meter that can perform datalogging and I think it is a powerful feature because when it is needed this ability will save a lot of work.  It seems I often need to design new types of sensor Many of these sensors need to be tested for linearity and accuracy This usually involves manually adjusting or sometimes automatically adjusting a quantity to be measured and taking corresponding readings to be analyzed later It is always tedious and time-consuming to stop manipulating th ...
One of the applications I wanted to include in this road test is capacitance water level sensors because you can get an accurate depth measurement for almost no cost as long as you have a meter that can measure capacitance The Keysight  U1282A meter does measure capacitance and is useful for testing and calibrating such sensors The physics behind why this technique works is a little trickier than it looks but I want to provide a bit of a feel for the technique without delving into math Basi ...
This segment of the road test will start exploring some of the applications I want to use this meter for - the real reasons I applied for the road test.   I design and assemble a lot of PCBs with surface mount components. Inevitably I end up with a variable number of random unused parts of unknown value. Capacitors in particular or small footprint resistors have no markings to indicate their value, so these parts become essentially useless. I have collected a small container with quite a nu ...
The Keysight  U1282A Multimeter is an awesome instrument loads of features great resolution(59999 great accuracy(0.025 spectacular battery life(up to 800 hours and phenomenally rugged(3 m drop and IP67 Dave Jones has done a monumentally punishing torture test of this meter. Here he is tossing it out the window of a car driving at 88 km/hr and it still worked fine afterwards. If you want check out just how spectacularly rugged this meter is see his torture test video here. Maybe Keysight ...
This is the third installment in the Keysight  https://www.element14.com/community/view-product.jspa?fsku=NULL&nsku=58Y5948&COM=noscriptU1282A digital multimeter road test In this segment I am exploring some of the capabilities and procedures that allow this meter to measure voltage waveforms.   Links to other installments of this road test: unboxing component and DC voltage measurements exploration waveform measurements exploration teardown research applications exploration ...
This is the second installment in the Keysight  U1282A digital multimeter road test In this segment I am exploring some of the capabilities and procedures that allow this meter to measure component values and DC voltages   Links to other installments of this road test: unboxing component and DC voltage measurements exploration waveform measurements exploration teardown research applications exploration - component sorting applications exploration - water level measurement applicatio ...
The Keysight  U1282A has just arrived for a road test It has been a long tough week but I wanted to get started on the road test with an unboxing video I intend to add more blogs and video to this review but I will edit this blog to add all the links as they get completed Note the handy storage clips for the probes, that protect the probe tips and control the leads while not in use. Those probe slots provide extra cushioning if the device is dropped. This instrument is quite large for a ...

Filter Blog

By date: By tag: