Skip navigation
Top Hardware Features Evaluation Setup the Oscilloscope for Measurements Experimenting with the SPI Protocol Testing the UART Protocol I2C Protocol Measurements Conclusion   Top Hardware Features Evaluation  This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Setup the Oscilloscope for Measurements    Fig: Setup the oscilloscope for measurements   Experimenting with the SPI Protocol  SPI or ...
Evaluating the Waveform and Pattern Generator Feature Specifications of the Waveform/function Generator in RTM3004 Testing the Waveform Generator in RTM 3004 Experiments with the Pattern Generator Evaluating the Waveform and Pattern Generator Feature This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Specifications of the Waveform/function Generator in RTM3004Fig: Specifications of the RTM Waveform Generator Testing the Wavefo ...
Software Control of the Oscilloscope Web-browser Control of RTM3004 Instrument Home Control of the Remote Front Panel Checking out the Live Screen USB Access of the RTM 3004 R&S Forum Control of the RTM 3004 R&S RSCommander display trace control   Software Control of the Oscilloscope  This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   The RTM 3004 oscilloscope control via Ethernet and USB has been ...
Power measurements and testing Voltmeter DVM Power measurements in the RTM 3004 Setup of the TPSM84A21 Power Module Measurements with the TPSM84A21 Power Module Spectrum analysis of the Output voltage Transient Analysis of the Output voltage Measuring with Digital Voltmeter in RTM 3004   Power measurements and testing Voltmeter DVM This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Here I setup an experiment to ...
This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   This page contains links to all the reference material that was used in the Road-Test of RTM 3004 Oscilloscope for further reading. This material has been collected by me during this road-test and is good for an in-depth understanding the state of the art functionality of an oscilloscope.   https://www.rohde-schwarz.com/us/product/rtm3000-productstartpage_63493-427459.html https://www.ro ...
This is a list of the external devices that were used to perform experiments during the road-test of Rohde & Schwarz Oscilloscope Kit RTM3K-COM4   List of Instruments Used in the Road-test Noise Generator Noisecom NC6110 Other Oscilloscopes used for verification of measurements GND Isolator Power Supply Rhode und Schwarz Signal Generator SML03 Tektronix CSA 803A   List of Instruments Used in the Road-test  Noise Generator Noisecom NC6110  The N ...
Noise Measurements Using R&S RTM3K Oscilloscope Setup for NULL Noise Measurements Measuring the oscilloscope noise floor RTM- 3004 Oscilloscope Noise as a function of Sensitivity Noise Comparison with Keysight Tektronix and LeCroy 1GHz Bandwidth MSOs Standard Noise Generator Noisecom NC6110   Noise Measurements Using R&S RTM3K OscilloscopeThis blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Noise plays an impo ...
Evaluating R&S RTM 3K Oscilloscope Bandwidth and Rise time Calculating the BW of R&S RTM FFT functionality Tests with the R&S Signal Generator Evaluating the fastest Rise time (tr) of R&S RTM 3004   Evaluating R&S RTM 3K Oscilloscope Bandwidth and Rise time  This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Calculating the BW of R&S RTM  The generic rule is that the oscilloscope bandwidth ...

Filter Blog

By date: By tag: