Skip navigation
When I first read about the Omron HVC-P2 roadtest I was excited about the possibility of implementing a security monitoring application with a camera/image processor that had human image recognition built in.  Based on the specs I thought I could monitor an area 20 feet deep by 10 feet wide (about the size of either the outside or inside entry area to my house).  I discussed the applicable parameters in my "Application Feasibilty" blog post.  As I've been testing the unit, I've co ...
Road-Test Blog 3 from MyIoT: Infineon Shield2Go Boards for IoT - Review   Here I used the Wemos mini D1 module and interfaced the 3D magnetic sensor TLV493D-A1B6 & DPS310 Pressure Sensor via I2C bus. I broke the mini board of 3D sensor head for portability. But the mini DPS310 head can only communicate via 3 wire SPI and not I2C. The Infineon Github repository has only I2C library for the DPS310 Pressure Sensor so I decided to keep the whole sensor board. The Wemos communicates via the ...
This is a next blog from the Road-Test Part2 MyIoT: Infineon Shield2Go Boards for IoT - Review   Installing DAVE4.0 LED BlinkyTest with Dave4.0 and XMC1100 BootKit Working with Arduino UNO and S2Go sensors Testing XMC1100 and S2Go sensors with Arduino IDE   Installing DAVE4.0  DAVE is a professional development platform for XMC microcontrollers from Infineon. It uses the the Eclipse IDE and is loaded with different software examples. I also tested the Infineon ...

Filter Blog

By date: By tag: