Skip navigation
Welcome to All Parents and K-12 Teachers to the element14 RoadTest Program!   The element14 RoadTest & Reviews program has traditionally been an engineering-product program where free products are given to element14.com community members in exchange for a detailed review or project that incorporates the product. But over the past year (2018), we have expanded the program to include more STEM products that could be used in the classroom by K-12 teachers, or in the home where parents and ...
The Drawing Robot from Arduino Engineering Kit   Currently dealing with the technical programming issues... tbd.... ...
I have only very recently started participating in the Element14 community and so was really pleased and excited to get picked for my first RoadTest on the AVR-IoT WG Development Board!   Participating in a RoadTest has certainly kick-started me into getting involved on here...... Thankyou to rscasny for recommending my application for this RoadTest! I was waiting with excitement and anticipation to receive the board - which took a little longer as it was sent from the US to the UK where ...
After spending many hour this week working with the MiniZed, I have in mind a few discussion points to ponder...... 1) Why aren't there any MiniZed community projects on the Zedboard.org site? Is this board not popular, or obsolete already? I look at all the available example projects for Arduino and Raspberry Pi and wonder. 2) Is the Zynq platform just too complicated/time consuming for most hobbyists? The amount of HD space required for the toolchain is enormous, and a fast machine is re ...
I use an Arduino Mega ADK with a dated can bus shield v1.1   the can bus shield library is downloaded from https://github.com/Seeed-Studio/CAN_BUS_Shield the i modify the example received_check , to change the pin to 10 instead of the original 9 const int SPI_CS_PIN = 10;   this will shows init success on Arduino serial monitor.   In picoscope       i actually try to add another channel, but unsure why the CAN low cannot decode any signal. i decide to fi ...

Filter Blog

By date: By tag: