Skip navigation

RoadTests & Reviews

4 Posts authored by: rsc
I had a break in my schedule, so I filled the water tunnel to see how the Eaton breaker was doing. I set up the controls to run a typical experiment. The first observation is that the Eaton breaker didn't register any current draw on the meter below 1 amp. The usual way of controlling the motor is by setting the motor control frequency as a percentage of maximum. My starting frequency for an experiment is around 4hz and the maximum is around 25hz. The Eaton breaker didn't show 1A until app ...
I've been pondering how to utilize the features of the Power Defense Circuit breaker. Here's a link to the Eaton site for this breaker https://www.eaton.com/us/en-us/skuPage.PDG23F0060P2MJ.html The first challenge was to figure out all the loose wires coming out of the sides of the breaker. There was no wiring instructions provided with the unit. I figured out a few of the lines from online data sheets:   Eaton Power Defense molded case circuit breaker, Globally Rated, Frame 2, Th ...
I'll need to do this road test in parts, because it may get complicated. The first task is installation.  This will require removal of the existing breaker and replace it with the Power Defense breaker. The PDG23F0060P2MJ is a frame size larger than the existing breaker, so that may be a challenge. Here is the existing breaker: Here is the enclosure: The PDG23F0060P2MJ arrived in a well packaged box. The contents were a PDG23F0060P2MJ, 4 mounting screws, a manual of sorts, a ...
After spending many hour this week working with the MiniZed, I have in mind a few discussion points to ponder...... 1) Why aren't there any MiniZed community projects on the Zedboard.org site? Is this board not popular, or obsolete already? I look at all the available example projects for Arduino and Raspberry Pi and wonder. 2) Is the Zynq platform just too complicated/time consuming for most hobbyists? The amount of HD space required for the toolchain is enormous, and a fast machine is re ...

Filter Blog

By date: By tag: