Skip navigation
1 2 Previous

RoadTests & Reviews

20 Posts authored by: snidhi
This road-test is a continuation from Keithley Bench Digital Multimeter - Review   In this blog I played around and investigated the KickStart Instrument PC Control Software for data collection and plotting graphs with DMM 6500.   Evaluate the KickStart software usability for beginners Automate measurements from DMM6500 using KickStart Using Test Script Builder (TSB) Conclusion   Evaluate the KickStart software usability for beginners  KickStart software ...
This road-test is a continuation from Keithley Bench Digital Multimeter - Review   Here I did some experiments to verify the core features of the Keithley DMM6500. These are some analog experiments to test the functionality.   dcv:dcv Ratio Measurements Check AC voltage at mains supply Measure capacitance Measure Resistance The internal probe resistance Test diode functionality Conclusion   dcv:dcv Ratio Measurements This measurement will be done by ...
This road-test review is a continuation from   All Reference Material for Keithley Benchtop DMM6500   https://uk.tek.com/tektronix-and-keithley-digital-multimeter/dmm6500 https://uk.tek.com/tektronix-and-keithley-digital-multimeter/dmm6500-manual/model-dmm6500-6-1-2-digit-multimeter https://uk.tek.com/tektronix-and-keithley-digital-multimeter/dmm6500-manual/model-dmm6500-6-1-2-digit-bench-system-0 https://uk.tek.com/tektronix-and-keithley-digital-multimeter/dmm6500-manual/model-dm ...
This blog is a continuation from Keithley Bench Digital Multimeter - Review   This is an experiment to measure the low current of the solar panels. I have a single solar panel of 5V and roughly 500 mA current output capability. I want to test them under different minimum light conditions to see the lower currents in the solar panel. This is to analyze the current output of the solar panels in milliamps range. As I have not put the solar panels in the sunlight I have not used any protectio ...
Road-Test Blog 3 from MyIoT: Infineon Shield2Go Boards for IoT - Review   Here I used the Wemos mini D1 module and interfaced the 3D magnetic sensor TLV493D-A1B6 & DPS310 Pressure Sensor via I2C bus. I broke the mini board of 3D sensor head for portability. But the mini DPS310 head can only communicate via 3 wire SPI and not I2C. The Infineon Github repository has only I2C library for the DPS310 Pressure Sensor so I decided to keep the whole sensor board. The Wemos communicates via the ...
This is a next blog from the Road-Test Part2 MyIoT: Infineon Shield2Go Boards for IoT - Review   Installing DAVE4.0 LED BlinkyTest with Dave4.0 and XMC1100 BootKit Working with Arduino UNO and S2Go sensors Testing XMC1100 and S2Go sensors with Arduino IDE   Installing DAVE4.0  DAVE is a professional development platform for XMC microcontrollers from Infineon. It uses the the Eclipse IDE and is loaded with different software examples. I also tested the Infineon ...
Top Hardware Features Evaluation Setup the Oscilloscope for Measurements Experimenting with the SPI Protocol Testing the UART Protocol I2C Protocol Measurements Conclusion   Top Hardware Features Evaluation  This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Setup the Oscilloscope for Measurements    Fig: Setup the oscilloscope for measurements   Experimenting with the SPI Protocol  SPI or ...
Evaluating the Waveform and Pattern Generator Feature Specifications of the Waveform/function Generator in RTM3004 Testing the Waveform Generator in RTM 3004 Experiments with the Pattern Generator Evaluating the Waveform and Pattern Generator Feature This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Specifications of the Waveform/function Generator in RTM3004Fig: Specifications of the RTM Waveform Generator Testing the Wavefo ...
Software Control of the Oscilloscope Web-browser Control of RTM3004 Instrument Home Control of the Remote Front Panel Checking out the Live Screen USB Access of the RTM 3004 R&S Forum Control of the RTM 3004 R&S RSCommander display trace control   Software Control of the Oscilloscope  This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   The RTM 3004 oscilloscope control via Ethernet and USB has been ...
Power measurements and testing Voltmeter DVM Power measurements in the RTM 3004 Setup of the TPSM84A21 Power Module Measurements with the TPSM84A21 Power Module Spectrum analysis of the Output voltage Transient Analysis of the Output voltage Measuring with Digital Voltmeter in RTM 3004   Power measurements and testing Voltmeter DVM This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Here I setup an experiment to ...
This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   This page contains links to all the reference material that was used in the Road-Test of RTM 3004 Oscilloscope for further reading. This material has been collected by me during this road-test and is good for an in-depth understanding the state of the art functionality of an oscilloscope.   https://www.rohde-schwarz.com/us/product/rtm3000-productstartpage_63493-427459.html https://www.ro ...
This is a list of the external devices that were used to perform experiments during the road-test of Rohde & Schwarz Oscilloscope Kit RTM3K-COM4   List of Instruments Used in the Road-test Noise Generator Noisecom NC6110 Other Oscilloscopes used for verification of measurements GND Isolator Power Supply Rhode und Schwarz Signal Generator SML03 Tektronix CSA 803A   List of Instruments Used in the Road-test  Noise Generator Noisecom NC6110  The N ...
Noise Measurements Using R&S RTM3K Oscilloscope Setup for NULL Noise Measurements Measuring the oscilloscope noise floor RTM- 3004 Oscilloscope Noise as a function of Sensitivity Noise Comparison with Keysight Tektronix and LeCroy 1GHz Bandwidth MSOs Standard Noise Generator Noisecom NC6110   Noise Measurements Using R&S RTM3K OscilloscopeThis blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Noise plays an impo ...
Evaluating R&S RTM 3K Oscilloscope Bandwidth and Rise time Calculating the BW of R&S RTM FFT functionality Tests with the R&S Signal Generator Evaluating the fastest Rise time (tr) of R&S RTM 3004   Evaluating R&S RTM 3K Oscilloscope Bandwidth and Rise time  This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review   Calculating the BW of R&S RTM  The generic rule is that the oscilloscope bandwidth ...
EA LPC11U37H Board with ulinkplus debugger in KEIL uVision   The (EA) Embedded Artists OM13074 LPCXpresso LPC11U37 board has been used for tests here. As one can see this board also has another version OM13062 which is sold by NXP and not EA.   In the EA LPC11U37H LPCXpresso Board Schematics I checked that the board is supported by 10-pin, 0.05" SWD connector. The pinout for the SWD connector can be seen in the first page of the blog. This board is powered by USB and ARM ulink plu ...

Filter Blog

By date: By tag: