Skip navigation
Will the V2 Tracking SDK improve on Leap Motion’s not so stellar performance? (via LeapMotion) Since Microsoft released their Kinect motion-tracking controller back in 2010, companies have been clamoring to bring their own gestural interfaces to the market. ASUS was one of the first to recognize the future of interaction and began developing their Xtion motion-sensing device, which incidentally was created by the same engineers responsible for the Kinect and features much of the same ...
  MotionSavvy’s Beta translator program running on an Android tablet (via MotionSavvy) A team of deaf student from the University of Rochester recently teamed up with Leap Motion to create a device that can translate American Sign Language (ASL) into spoken words to better help the deaf communicate with the world around them.   More than 70 million people in the United States are deaf. The vast majority, 90 percent of these persons are born into hearing families, making co ...
Have you ever stood in an agonizingly long line and wondered if there would ever be a faster way to pay for transactions than counting all the pennies in your piggy bank, one-by-one? Well, thanks to students at Lund University in Sweden, now there is – simply, pay with your palm.   A team of Lund students, led by engineering student Fredrik Leifland, designed a new palm scanner that distinguishes each person’s identity through the unique pattern of veins in a person’s ha ...
Ever wanted to control your devices without the need to actually touch them? Turn on a light with the wave of your hand or control your music player with the flick of your finger. Designing with the GestIC© technology from Microchip makes all these possible.   We have partnered with Microchip to bring you the first 3D Gesture RoadTest Plus!   All you need to do is submit a proposal stating why you would like to review this product in your RoadTest application. If you are c ...
The mould will be used for casting concrete. For this project I will use 2 mould sizes; 2” dia. and 4” dia. with a height of 5”. Rebar samples will have 6” in length. Concrete will be poured into the mould with a rebar (steel) in the middle. Inductance readings will be taken on these specimens. ...
Join us at Stand 12-264 at Sensor+Test   MSS Piezo Technologies will be exhibiting at the Sensor+Test conference in Nurnberg, Germany June 3-5, 2014.  At stand 12-264, Piezo Technologies' ultrasonic measurement solutions will showcased through a live demonstration.   About Sensor+Test The SENSOR+TEST 2014 from the 3rd to the 5th of June in Nürnberg is more than just a trade fair: Besides the exhibition itself, the extensive action program offers visitors numerous other ...
This week I received the kit but I had to pay PHP 515.00 to UPS.  I acquired the permit to use the Material Testing Laboratory of Mindanao State University - Iligan Institute of Technology. ...
Hello! Good day! Before i start let me thank element14, texas instrument, cadsoft for selecting my idea and sponsoring my project idea, Let me break my crazy little idea i wish to do with Inductive sensor. Is measuring haemoglobin level in our blood using this touchless Inductive sensor. As you all know our blood is made of iron. So i consider that as conducting material. Now inorder to get something from it. I first give a magnetic flux/filed to a specific part of our body say finger. Now ...
Overview Steel is one of the major components in building construction because of its constructability and strength. It provides tensile strength capacity to a structural concrete. The combination of steel and reinforced concrete offers a great deal in construction building considering the cost, strength/weight ratio, constructability, sustainability, and etc. To determine the strength of a steel, a sample undergoes tensile test. This is the common method used in Civil Engineering. However ...

Filter Blog

By date: By tag: