Skip navigation
The DADSS programs hopes to put an end to drunk driving, with a technology that prevents a drunk driver from driving when intoxicated. The project involves the development of a car that tests blood alcohol content (BAC) and prevents ignition-start up when a driver’s BAC is at or above 0.08. Will you be stranded every weekend? (via dadss.org) We all know we are not supposed to drive drunk, but people still do. According to the CDC, in 2013 roughly 31% of all traffic-related deaths invo ...
These drum pads and foot pedals fit over and under your clothes. DrumPants 2.0 has new features and will be open source? (via Drumpants) Rhythm games such as Rock Band and Guitar Hero are making a triumphant return this year. But if you want to feel like a rock star without holding plastic instruments and pressing buttons, then DrumPants may be what you're looking for. First introduced in 2007 by Tyler Freeman, DrumPants are a set of accessories made of two elongated drum pads and two foot ...
TU Wien Researcher. A research team from the Vienna University of Technology and Vienna Medical University recently developed a polymer-based artificial blood vessel that promotes the natural growth of a new one, so that when the polymer dissolves and a patient is left with a brand new, healthy blood vessel. (via TU Wien)   As a nation plagued by heart attacks and heart disease, there is no lack of demand for emerging technology that can save lives. That’s why the Vienna University ...

Filter Blog

By date: By tag: