Skip navigation

Sensors

7 Posts authored by: rscasny element14 Team
Collaborative robots, or cobots, are robots that can work alongside or with humans. These cobots are intended to interact with and assist workers as opposed to being standalone automated equipment with little to no human interaction. Historically, this limited interaction was due to safety concerns and the fact that humans and robots were not able to work together effectively and efficiently.   Today, cobots offer much greater flexibility in the workplace since protective cages are no long ...
There's 10 days to go to enroll in the Experimenting with Vibration Sensors Design Challenge.   You can apply by going here: https://www.element14.com/community/community/create-roadTestApp!input.jspa?containerID=3071&containerType=14&roadTestID…   About Experimenting with Virbration Sensors Vibrations are periodic motions or oscillations that occur naturally or emanate from many types of mechanical and electromechanical systems and devices. Earthquakes produce vibrati ...
Bourns introduced a new environmental pressure sensor model that provides high accuracy, 3.3 V and ultra-low pressure range capabilities. Bourns® Model BPS125 pressure sensors are based on state-of-the-art Micro-Electro-Mechanical Systems (MEMS) technology and deliver precision performance in a miniature package size. Designed for space-constrained, 3.3 V digital systems that demand extremely sensitive and accurate readings, Bourns® Model BPS125 is capable of measuring pressure in the ...
STMicroelectronics has introduced its IIS3DWB vibration sensor, supported by the STEVAL-STWINKT1 multi-sensor evaluation kit, that accelerates development of condition-monitoring systems that boost productivity by inferring equipment maintenance needs.   The IIS3DWB is a 3-axis MEMS1 accelerometer optimized for industrial vibration sensing. The STEVAL-STWINKT1 simplifies prototyping and testing by integrating the IIS3DWB with additional sensors, an ultra-low-power microcontroller and algor ...
Infineon announced its XENSIV™TLE5109A16  AMR-based angle sensors to address the need for very precise, fast and yet cost-efficient angle measurement at the highest functional safety levels in automotive and industrial applications. These include position measurement in brushless DC motors for pumps, wipers or brakes, position measurements of valves, flaps or pedals and steering angle measurement.   The new devices are designed for 180° angle measurement but are also applic ...
ON Semiconductor has introduced the ARX3A0 digital image sensor with 0.3 Mega-Pixel (MP) resolution in a 1:1 aspect ratio. With up to 360 frames per second (fps) capture rate it can perform like a global shutter in many conditions but with the size, performance and responsivity benefits of being a Back-Side Illuminated (BSI) rolling shutter sensor. With its small size, square format and high frame rate, ARX3A0 is particularly suitable for emerging Machine Vision, Artificial Intelligence and AR/V ...
Vishay has brought out RGBC-IR sensors for applications such as automatic white balancing and color cast correction in digital cameras; automatic LCD backlight adjustment; and active monitoring of LED color output for IoT and smart lighting. The new VEML3328 (top-looking) and VEML3328SL (side-looking) sensors offer improved linearity and higher sensitivity, as well as new features including an infrared (IR) channel.   The sensors sense red, green, blue, clear, and IR light by incorporating ...

Filter Blog

By date: By tag: