Skip navigation
Choosing the right inspection system for your application can be a daunting task.   For industrial applications 3 types of inspection systems are generally used.   This blog describes these systems, their common applications along with pros & cons.   Stereo Zoom Microscope  The stereo zoom microscope is the most commonly used microscope in industrial applications.   A stereo scope generally consists of a main objective lens, two eyepieces for viewing with a magni ...
Real estate is at a premium in the lab. I don't have much bench space for test gear. That's why I purchased a Metex test system. It's a DMM, 3 power supplies, a function generator and a counter in one box.     I bought it second hand. It was owned by someone who stopped his electronics studies.   Left Side: Function Generator and Universal Counter  The generator and counter can be used separately, but it's also possible to let the counter show the settings of the functi ...
Dave Jone's Of The EEVBLOG did some posts on a DIY PSU around a year back. This project is a spin off of that and I made some changes according to my liking and finally made a PCB that I can use. There are still some things that need to be done. I made a small video for the same which is linked below.     The major differences in this version are as follows: 1. Voltage reference is 4.096V 2. Buttons for interface. 3. Cheaper LCD. 4. 10 1Ohm Resistors   Will share schem ...
I hope this post would not cause complete and total exclusion of myself from Roadtest thing, but posting it here anyway, for fellow engineers enjoyment In this prompt we will take a look on Fluke 51-II and try some ideas how to improve it by modifications User manual for meter is available here Feature comparison  Before we go any further, Fluke 50 II series thermometers specs:   51 II features 52 II features 53 II features 54 II features Amount of channels     ...

Filter Blog

By date: By tag: