Skip navigation
Disney Research has created a system that uses fewer sensors, provides a greater range of motions, and is easier to set up. A demonstration on the new motion capture system works (Screencap from Disney)   Motion capture is a great source for making animation so life like. Their fluid motions and movement are the result of someone in a motion capture suit. Though it’s made some facets of animation easier, it’s not easy to set up in itself. We’ve all seen the motion capture ...
Motorola Mobility CEO Aymar de Lencquesaing stated the Moto Z would likely have a Tango-based Mod. (via Lenovo)   By now, you’ve probably heard of Google’s Tango technology but for those who haven’t, it’s essentially a form of computer vision that allows mobile devices to gain spatial awareness and detect their relative position in any given environment without using external signals. This makes for some great applications such as 3D mapping, VR, indoor navigation a ...
Two students from the University of Genoa created a headset that uses cameras to help the visually impaired see and read. This headset looks more like an MP3 player, but is actually a device to help the visually impaired (Via Horus)   Machine learning has made everything smarter from our cars to even our houses. The simplest tasks can now be performed with a simple command or tap of a button. But machine learning is not only being used to make our lives easier; it can also help those who a ...

Filter Blog

By date: By tag: