Skip navigation

Test & Tools

3 Posts authored by: jadew
     Hello everyone,        One of the uses the Agilent 33622A can have, is that of a signal source in an automated test system. Automated test systems are used on the production lines to test for defects, in the research stage for design validation (running a bunch of tests and checking if the result is within the expected limits), for characterization of a DUT and so on.        While you can connect to the instruments dire ...
    Hey guys,       For this blog post, I decided to show how I used the Agilent 33622A Waveform Generator to design and test a small piece from a bigger project I'm working on and use it to prove a technique of increasing ADC resolution by turning noise into an advantage, via oversampling and decimation. The ADC trick should come in handy to anyone new to MCUs, because they often run into the issue of low resolution and noisy readings and usually, they have n ...
    Hello guys,       I'm not entirely sure how these blog posts should look like, but I'm going to give it a try and hope I won't be off by too much. I figured I should play a little with PRBS and tell you what I did, since it's one of the most prominent features of the Agilent 33600A series and maybe shed some light on why and when it's needed, so those of you who didn't know about this until now, can make a more informed decision when you're going to buy yo ...

Filter Blog

By date: By tag: