Skip navigation
Batemika Measurement Solutions was able to improve the accuracy of its UT-ONE family of thermometer readouts by implementing a VHP101T Hermetically-Sealed Bulk Metal® Foil resistor as the internal reference resistor. Long-term drifts were improved from over 20 ppm per year to less than 5 ppm per year.   Case study link:  http://www.vishaypg.com/foil-resistors/case-studies/study/batemika_1/ ...
FNP Series by Alpha Electronics has been listed as one of the top test & measurement products of the year!     EDN100 Test and Measurements page: https://www.edn.com/electronics-products/other/4459147/EDN-Hot-100-products-of-2017--Test---Measurement     FNP  High-Power Precision Shunt Resistors Incorporating Bulk Metal Foil Technology review: https://www.edn.com/electronics-products/other/4458350/Foil-shunt-resistors-contain-integrated-RTD     PR: http: ...
The HRU standard resistors (10 ohm and 100 ohm) will be formally used on the Watt Balance system for mass standard which has been developed by NIST (US) and NRC (Canada) as next generation’s mass standard unit from 2018. At Watt Balance system, current (A) and voltage (V) are extremely important as these enable researchers to determine the mass of an object indirectly via two measuring modes: the strength of the magnetic field, and the current running through a coil of wire. For this appli ...
Inexpensive, precise, stable and rugged, the most practical solution for RTD simulation: Bulk Metal Foil trimmed to the exact value of PT100 @ +125C, 147.952 ohms.    iNotes-quick webinar:  http://bit.ly/2xfpQrN   RTD Simulators – Product sheet: http://www.vishaypg.com/doc?63524   Resistor technical datasheet: http://www.vishaypg.com/doc?63255 ...
The VPG Foil Resistors product group of Vishay Precision Group (NYSE: VPG) (www.vpgfoilresistors.com), manufacturers of the industry’s most precise and stable precision resistors, introduced the Model 303337 ultra-high precision military and space-grade resistor, offering high-performance current sensing within mission-critical applications (based on resistor model/type CSM3637F).    The Model 303337 produces a highly precise voltage that is directly proportional to measured cur ...
Vishay Foil Resistors has released a new demo highlighting the inherent long-term stability of VPG Bulk Metal Foil resistors. http://bit.ly/1PPcya6 ...

Filter Blog

By date: By tag: