Skip navigation
1 2 3 Previous

Wireless Power Solution

37 posts
Würth Elektronik eiSos brings you the latest: Wireless Power Consortium (WPC) expands standard The WPC announced the addition of the 15-W and "multi-device charging" options to the Qi standard. Draft versions of the specs were released to its members. http://www.wirelesspowerconsortium.com/data/downloadables/1/3/6/2/technology-milestones-for-fast-charging-and-resonant-multi-device-charging-with-spatial-freedom.pdf   Würth Elektronik eiSos, as Full Member of the WPC, welc ...
sleuz

Win a Wireless Power Kit

Posted by sleuz Aug 6, 2014
Go to http://www.we-online.de/web/en/electronic_components/extra_pbs/umfragewirelesspower.php and win a wireless power kit from Würth Elektronik! ...
My previous summaries can be found here: All Turning Up Shiny - The Wireless Power Challenge 2014 Down with Cables ! - The Wireless Power Challenge 2014 Electrifying - The Wireless Power Challenge 2014 Tesla would be Proud - The Wireless Power Challenge 2014 Weeee - The Wireless Power Challenge 2014 Progress ! - The Wireless Power Challenge 2014 It Starts ! - The Wireless Power Challenge 2014     Name Super Awesome Blog Time Janis Alnis No Updates. Mark Beckett Beyond the Phone ...
University of Illinois and Northwestern University’s health-monitoring patch (via UI) Wearable electronics (or computing) have become quite popular since the first armband was marketed for the iPod about a decade ago. Recent years have seen the rise of devices such as Google Glass, Sony’s SmartWatch and Nike’s Hyperdunk+ basketball shoes just to name a few of the wearable tech that’s currently on the market. Another rise in popularity among wearable electronics cente ...
WiT3300 evaluation kit (via Witricity) When we think of the wireless transmission of energy, we typically think of Tesla and his giant iconic coil sparking electric discharge. The idea he had was to bring wireless energy to every part of the world that could be used to power everything from trains to airships. Fast-forward a hundred years or so and the idea of transmitting wireless power has been realized but on a much smaller scale. Instead of providing wireless power to the world, we can ...
Here's a video of the unboxing of the Wireless design kit. Enjoy!!     The kit was very well packed, and boasts the same amount of test points as the previous version.   Do use the supplied adapter when powering it, as this baby could pull 5W, and your laptop supply might not be able to deliver that. I'll do a comparison between this system and the one I used at the previous design challenge somewhere next week! ...
Wireless Power Transfer Solution To Go     Texas Instruments and Würth Elektronik put together the Wireless Power Transfer Solution to Go Evalkit, which can be used as a full-featured development platform right out of the box. You can immediately connect the receiver to the power management of your device and wireless power comes to life. The kit offers a variety of programmable parameters to set your wireless power transfer.   The Wireless Power Transfer Solution To Go pr ...
Wireless Power Consortium extends Qi standard to add resonance charging  In a press release the Wireless Power Consortium, custodian of the Qi wireless charging standard widely used in Nokia handsets, has announced it has added Resonance Charging to their Qi protocol. The Qi resonant extension will allow charging with higher efficiency and lower radio frequency interference than typical resonant solutions. In addition, the extension allows for multiple device charging and charging at long ...
Brando Wireless Power Bank 4800mAh reviewby Julie Strietelmeier from the gadgeteer     I like products that make my life easier and save me time, even if it’s only a couple seconds. The Wireless Power Bank 4800mAh from Brando ticks both of those boxes. It’s a wireless charger that uses Qi (pronounced “Chee”) inductive charging. Some of the latest mobile devices like the Nexus 7 2013 tablet and LG G2 Android smartphone have Qi built in. Other devices require a ...
The Smallest Qi-Enabled Wireless Charging Pad Is Released by EsorunThis stylish round Qi-enabled wireless charging pad is the smallest wireless transmitter whose size is only 58(D)*10.4(T)mm. Elf possesses a built-in USB cable and is a green DIY wireless charging product with its Qi 1.1 technology.wireless charging The Stylishest Wireless Charging Pad ELF   The smallest Qi-enabled wireless charging pad got released by Esorun. Since the release of internal testing samples, all individuals h ...
Pre-order your Glowdeck now power - light - sound     Smartphone users on the lookout for battery-powered wireless chargers, Bluetooth music players, and funky smart lights that bop to the beat will likely have to settle for a small collection of separates. There are devices that tick a couple of boxes, such as the Black Diamond III or TDK's Wireless Charging Speaker, but good luck finding one unit that does it all. If Justin Kaufman's new crowdfunding endeavor is successful, ...
Monster Watts, an innovator of mobile phone wireless charging accessories, is introducing the 5 in 1 iQ View wireless charging flip cover for the Samsung Galaxy S4.   Despite the light and thin design, it still manages to combine: Wireless charging receiver Interactive quick view window Battery saver Screen protector Phone case     Wireless Charging Thin wireless charging receiver is integrated into the back cover, and works with any Qi compatible charging pads * NFC ...
  Here we’re having a look at a set of new Nokia devices, one of the most instantly appealing being the universal NFC Wireless Car Charger. This device is made to work with the Lumia lineup of Nokia devices first and foremost, of course, working with Qi standard wireless charging as well as embedded NFC to tell your device it’s docked. When you do dock a device like the wireless charging-shell CC-3068-toting Lumia 720, you’ve got wireless charging, NFC-activated car mode, ...
Monster Watts WiQiQi puts wireless charging in Samsung Galaxy phones without new cases Samsung already has wireless charging options for phones like the Galaxy S4, but they require a separate cover that adds a slight amount of bulk. For Monster Watts, that’s still too much. The company’s upcoming WiQiQi charging receiver is thin enough to slip under the existing cases of both the S4 as well as the Galaxy S III and Galaxy Note II, giving them the same Qi-based wireless power as offi ...
We’ve heard of bags that charge your gadgets — the Powerbag Instant Messenger comes to mind — but none targeted directly at women. That’s where the Everpurse comes in. It’s a Kickstarter project started by married couple Dan and Liz Salcedo. Essentially, you place your phone in a purse, or a purse insert (which is essentially a smaller bag you put inside your main bag), and it charges your phone on the go. Oh, and it’s entirely wireless. It works by using the ...