Monster Watts WiQiQi puts wireless charging in Samsung Galaxy phones without new casesQi_Logo.jpg

http://www.qiwireless.com/wp-content/uploads/2013/04/monster-watts-wiqiqi-gs4.jpg

Samsung already has wireless charging options for phones like the Galaxy S4, but they require a separate cover that adds a slight amount of bulk. For Monster Watts, that’s still too much. The company’s upcoming WiQiQi charging receiver is thin enough to slip under the existing cases of both the S4 as well as the Galaxy S III and Galaxy Note II, giving them the same Qi-based wireless power as official kits without disrupting the design or wrecking compatibility with accessories.


Kits for the two phones already on the market should be available soon. Monster Watts’ wire-free solution isn’t seamless, but it may be one of the more elegant in an era when wireless charging is only occasionally built-in.