Skip navigation
1 2 Previous

Wireless Power Solution

27 Posts authored by: sleuz
Würth Elektronik eiSos brings you the latest: Wireless Power Consortium (WPC) expands standard The WPC announced the addition of the 15-W and "multi-device charging" options to the Qi standard. Draft versions of the specs were released to its members. http://www.wirelesspowerconsortium.com/data/downloadables/1/3/6/2/technology-milestones-for-fast-charging-and-resonant-multi-device-charging-with-spatial-freedom.pdf   Würth Elektronik eiSos, as Full Member of the WPC, welc ...
sleuz

Win a Wireless Power Kit

Posted by sleuz Aug 6, 2014
Go to http://www.we-online.de/web/en/electronic_components/extra_pbs/umfragewirelesspower.php and win a wireless power kit from Würth Elektronik! ...
Wireless Power Transfer Solution To Go     Texas Instruments and Würth Elektronik put together the Wireless Power Transfer Solution to Go Evalkit, which can be used as a full-featured development platform right out of the box. You can immediately connect the receiver to the power management of your device and wireless power comes to life. The kit offers a variety of programmable parameters to set your wireless power transfer.   The Wireless Power Transfer Solution To Go pr ...
Wireless Power Consortium extends Qi standard to add resonance charging  In a press release the Wireless Power Consortium, custodian of the Qi wireless charging standard widely used in Nokia handsets, has announced it has added Resonance Charging to their Qi protocol. The Qi resonant extension will allow charging with higher efficiency and lower radio frequency interference than typical resonant solutions. In addition, the extension allows for multiple device charging and charging at long ...
Brando Wireless Power Bank 4800mAh reviewby Julie Strietelmeier from the gadgeteer     I like products that make my life easier and save me time, even if it’s only a couple seconds. The Wireless Power Bank 4800mAh from Brando ticks both of those boxes. It’s a wireless charger that uses Qi (pronounced “Chee”) inductive charging. Some of the latest mobile devices like the Nexus 7 2013 tablet and LG G2 Android smartphone have Qi built in. Other devices require a ...
The Smallest Qi-Enabled Wireless Charging Pad Is Released by EsorunThis stylish round Qi-enabled wireless charging pad is the smallest wireless transmitter whose size is only 58(D)*10.4(T)mm. Elf possesses a built-in USB cable and is a green DIY wireless charging product with its Qi 1.1 technology.wireless charging The Stylishest Wireless Charging Pad ELF   The smallest Qi-enabled wireless charging pad got released by Esorun. Since the release of internal testing samples, all individuals h ...
Pre-order your Glowdeck now power - light - sound     Smartphone users on the lookout for battery-powered wireless chargers, Bluetooth music players, and funky smart lights that bop to the beat will likely have to settle for a small collection of separates. There are devices that tick a couple of boxes, such as the Black Diamond III or TDK's Wireless Charging Speaker, but good luck finding one unit that does it all. If Justin Kaufman's new crowdfunding endeavor is successful, ...
Monster Watts, an innovator of mobile phone wireless charging accessories, is introducing the 5 in 1 iQ View wireless charging flip cover for the Samsung Galaxy S4.   Despite the light and thin design, it still manages to combine: Wireless charging receiver Interactive quick view window Battery saver Screen protector Phone case     Wireless Charging Thin wireless charging receiver is integrated into the back cover, and works with any Qi compatible charging pads * NFC ...
  Here we’re having a look at a set of new Nokia devices, one of the most instantly appealing being the universal NFC Wireless Car Charger. This device is made to work with the Lumia lineup of Nokia devices first and foremost, of course, working with Qi standard wireless charging as well as embedded NFC to tell your device it’s docked. When you do dock a device like the wireless charging-shell CC-3068-toting Lumia 720, you’ve got wireless charging, NFC-activated car mode, ...
Monster Watts WiQiQi puts wireless charging in Samsung Galaxy phones without new cases Samsung already has wireless charging options for phones like the Galaxy S4, but they require a separate cover that adds a slight amount of bulk. For Monster Watts, that’s still too much. The company’s upcoming WiQiQi charging receiver is thin enough to slip under the existing cases of both the S4 as well as the Galaxy S III and Galaxy Note II, giving them the same Qi-based wireless power as offi ...
We’ve heard of bags that charge your gadgets — the Powerbag Instant Messenger comes to mind — but none targeted directly at women. That’s where the Everpurse comes in. It’s a Kickstarter project started by married couple Dan and Liz Salcedo. Essentially, you place your phone in a purse, or a purse insert (which is essentially a smaller bag you put inside your main bag), and it charges your phone on the go. Oh, and it’s entirely wireless. It works by using the ...
  What is the similarity between the Toyota Avalon, Jeep Cherokee, Toyota Prius, and the Ssangyong Chairman? The Jeep Cherokee will offer a factory installed Qi wireless charging pad later this year. The optional feature -- located in the center console -- featuring technology developed by Leggett & Platt, is part of the optional Uconnect 8.4 package. To charge a Qi-compatible device, such as the Samsung Galaxy S4, HTC Droid DNA, or Nokia Lumia 920, customers simply place it in the m ...
Here is a live-talk on wireless power technology   ...
“Charge your smart phone or any other device that supports Qi on top of your night stand. It only took about 1 hour and 45 minutes to build using some tools. You could use almost any type of night stand but this one is from IKEA and therefore sold world wide and it comes in many colors. There are a number of methods to do this but I wanted to keep it as simple and quick as possible. You can take it to the next level by just carving around the charger and then drill a hole for the cable to ...
McDonald's testing Qi in EuropeRestaurants will install Qi wireless chargers in some of its European restaurants       McDonald's is testing wireless charging in partnership with Powerkiss, a Finnish company specialized in the design of very elegant solutions for embedding wireless chargers in furniture. Details are in the press release further down. Powerkiss' embedded Qi-chargers can be found in fancy locations all over Europe. Eric Bourgeois, Senior Director at McDonald's ...