13 Replies Latest reply on Sep 12, 2014 3:58 PM by pfinucan

    Unable to get anything working...

    pfinucan

      So I got my RiotBoard.  Plugged in keyboard mouse, hdmi, ethernet, and power.

       

      The andriod OS starts up but is mostly off the screen so it is unusable.  I can't get past the splash screen.  :-(

       

      UPDATE:  Got past the splash screen on andriod using this from the user manual

       

      Display with HDMI Only (Default mode)

      Execute the following instructions in u-boot mode to configure for HDMI display mode;

        MX6Solo RIOT U-Boot > setenv bootargs console=ttymxc1,115200

      init=/init nosmp video=mxcfb0:dev=hdmi,720x480M@60,bpp=32

      video=mxcfb1:off fbmem=10M vmalloc=400M

      androidboot.console=ttymxc1 androidboot.hardware=freescale

        MX6Solo RIOT U-Boot > saveenv

       

      For linux...

       

      I downloaded fsl-image-fb-riotboard.sdcard from dropbox (link is now gone) put it on a micro SD card.  Set the boot switch per the uSD settings (below).

       

                      D1 D2 D3 D4 D5 D6 D7 D8

      Serial Download  0  1  x  x  x  x  x  x

      SD (J6, bottom)  1  0  1  0  0  1  0  1

      uSD (J7, top)    1  0  1  0  0  1  1  0

      eMMC             1  0  1  1  0  1  1  1

       

      I get this in the debug terminal

       

      RPC: Registered udp transport module.

      RPC: Registered tcp transport module.

      RPC: Registered tcp NFSv4.1 backchannel transport module.

      hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

      pureg-dummy: no parameters

      Bus freq driver module loaded

      VFS: Disk quotas dquot_6.5.2

      Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

      NFS: Registering the id_resolver key type

      ....

      blah

      blah

      ....

      ALSA device list:

        #0: imx6q-sgtl5000

        #1: imx-hdmi-soc

      List of all partitions:

      b300         3751936 mmcblk0  driver: mmcblk

        b301            8192 mmcblk0p1 00000000-01

        b302            8192 mmcblk0p2 00000000-02

        b303               1 mmcblk0p3

        b304         2621440 mmcblk0p4 00000000-04

        b305          524287 mmcblk0p5 00000000-05

        b306          524287 mmcblk0p6 00000000-06

        b307            8191 mmcblk0p7 00000000-07

      b318             128 mmcblk0rpmb  (driver?)

      b310            2048 mmcblk0boot1  (driver?)

      b308            2048 mmcblk0boot0  (driver?)

      b320         7761920 mmcblk1  driver: mmcblk

        b321            8192 mmcblk1p1 00033ad3-01

        b322          544768 mmcblk1p2 00033ad3-02

      No filesystem could mount root, tried:  ext3 ext2 ext4 vfat fuseblk

      Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)

       

      Where can I get a linux img for an SD that works?  Like ANY image that boots.  Most of the links on the element14 or riotboard.org are dead.  How do you adjust the screen size on andriod? The whole thing is very frustrating.

       

      Can't use this guide...

      RIoTboard: Updating OS images in Windows Environment

       

      no tools...

       

      ....

      Not Found

      The requested URL /downloads/riotboard/tools_SVN2652.zip was not found on this server.

       

      Can't get the downlaods for this page:

      http://www.riotboard.org/index.php/download

       

      Not Found

      The requested URL /linux/Linux.zip was not found on this server.

       

      These links are only a few months old, how are they all gone already.  Anyway any help or suggestions would be great...