3 Replies Latest reply on Jun 29, 2020 5:25 PM by drozwood90

    An alternative for camera setup in Avnet Multicam4 FMC module

    aditya4822

      Hi,

      I am looking for an alternative hardware setup to replace the quad camera setup interfacing the Avnet multicam4 FMC module. This alternative setup should replicate the camera output and provide an image as input to the multicam4 FMC Module.

      Any suggestions or ideas will be really helpful.

      Thank you.

        • Re: An alternative for camera setup in Avnet Multicam4 FMC module
          drozwood90

          Hi there,

           

          I'm not sure I understand.  You want to use the FMC from the Quad Cam, but do not want to use the Cameras?  Did I understand that correctly?

           

          If that is the case, are you looking for something like a stack of USB cameras - or something like that?  It seems you want to have this output and image, like a still post processed?

           

          Any clarity will help me to help you.

           

          --Dan

          1 of 1 people found this helpful
            • Re: An alternative for camera setup in Avnet Multicam4 FMC module
              aditya4822

              Hi Dan,

              Yeah i want to use FMC from Quad cam and instead of camera image, i want to give my predefined image as an input to the FMC.

              This will help me to verify the working and compare the output with my  expected output.

              Is there any other hardware i can connect instead of the Quad cam setup through which i can give my predefined image input to the FMC?

              I hope this will clear some things.

              Thank you

               

              - Aditya

                • Re: An alternative for camera setup in Avnet Multicam4 FMC module
                  drozwood90

                  Hi there,

                   

                  It seems I lost the reply to this.  Sorry about that!

                  The camera FMC uses a specific method to bring camera information in.  If you wanted to replicate that you can, but the board was designed to operate with the cameras which are part of that kit.

                  You are of course free to use any input and with some gstreamer trickery, really could be just about anything including a file from the file system.  For example, we have a design for the UltraZed-EV that uses a USB webcam as input.

                   

                  --Dan

                  1 of 1 people found this helpful