This content has been marked as final.
Show 2 replies
-
Re: Which pad should I use for hand assembly ? C2106 or C2106K
dougwJan 3, 2021 9:06 AM (in response to spitfireant)
They both have lots of room for manual soldering and they are pretty much the same length.
I would use the smaller footprint.
-
Re: Which pad should I use for hand assembly ? C2106 or C2106K
Jan Cumps Jan 3, 2021 10:49 AM (in response to spitfireant)If you use paste, there's no need for "manual style" pads.
Go to original post
Reply to original post
Hi all,
I am trying to make my mind up about which pad I should use for placing capacitors or other devices using just my hot air gun.
Is there any advantage of choosing a C2106 over a 2106K for example?
I see the K is marked for reflow and see it's a little bigger.
Is that the only advantage ? ie: More paste ?
Why would I choose one over the other they both seem to work ?