-
Re: Change "Show" highlight color?
Autodesk Guest May 28, 2014 12:13 AM (in response to silica10)Am 28.05.2014 00:47, schrieb silica10:
Is there a way to change the "Show" function's highlight color? The
slightly lighter green when clicking on a wire doesn't make for a huge
difference from the darker green already there.
I'm using version 6.5.0. Light on a Mac.
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/114255
In options/settings you find 3 colour palettes for black, white and
coloured background. Here you can set or generate your own colours.
1st row is for the normal colours, 2nd row for the highlighted colours
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
-
Re: Change "Show" highlight color?
silica10 May 28, 2014 3:41 AM (in response to Autodesk Guest)Unfortunately this didn't work.
First I found out that there's an "Option" menu available while in the control panel window, and there's another "Option" menu which is only displayed when a schematic is open. This is where I found a sub-menu named "Set" which looks like this:
So next I clicked on the "colored background" button and changed it to some other colour but when pressing "OK" it didn't change!?!?!
But the "Dots" and "Lines" grid allowed for changing to other colours. I can't find anything for the "Info" function.
I've also tried the "View"-"Layers" menu (also only available when having opened a schematic), and see that "Info" is gray for some reason, but changing this to say, yellow doesn't make any difference. Wires are still light green when clicking with a "Show".
If it works for you, are you on a different version/platform than me?
I'm using 6.5.0. Light (freeware version) on the Mac OSX platform.
-
Re: Change "Show" highlight color?
dukepro May 28, 2014 8:50 AM (in response to silica10)In summary, each layer is assigned a color from a palette of 64 colors,
and you can set each color in a palette to any color you wish.
In your example, let's start with setting the palette.
From the schematic editor, click on Options->Set. Under the "Colors"
tab (which should be the default), click on color square to the right of
"White background" and under "Palette". A color selector dialog will be
presented.
On this, you will see 64 color squares, most of which are left at a dark
grey. The first row represents colors when they are NOT highlighted.
The second row represents colors when they ARE highlighted (as they are
with SHOW). Thus, when a net on a schematic is NOT highlighted, it
assumes the color in the first row and the third column. When it IS
highlighted, it displays as the color in the second row, same column.
This pattern is followed for any of the colors - highlighted colors are
in even number rows.
If you click on the highlighted green color square (row 2, column 3),
you can change this to any color you want. HSV, RGB, and transparency
(alpha channel) all can be set to your liking. Since the background is
white, you may choose to select a darker color to provide more contrast
with the background.
Now, that your palette has been set, you can assign specific colors to
each layer.
Again from the schematic editor, click on the "Layer settings" icon or
type DISPLAY into the command line. The first displayed layer is layer
91 named "Nets". Click on the color square, then click on the "Change"
button. This opens the "Change layer properties" dialog in which you
may choose any of the 64 colors defined in the palette. It is strongly
advised that you select a color from one of the odd rows. If you choose
a color from an even row, objects in the layer will not change color
when highlighted.
So, the palette defines a set of 64 colors, and the layer properties
defines which color to use from the palette.
With this in mind, note that there are three different palettes. One
for white backgrounds, one for colored backgrounds, and one for black
backgrounds. The actual color of the background is always the color in
row 1 column 1 of the respective palette. So the terms "black",
"colored", and "white" when referring to palette selection can be set to
any color you want, though the name of the palette is constant.
The palette to use for each of the layout and schematic editors can be
selected from Options->User Interface. There you'll see panels for each
of these editors allowing you to select the which background you prefer.
I believe, though I have not tested this, that the library editor uses
the schematic palette when editing symbols, and the layout palette when
editing packages.
Hope this helps,
- Chuck
On 05/28/2014 04:39 AM, silica10 wrote:
Unfortunately this didn't work.
First I found out that there's an "Option" menu available while in the
control panel window, and there's another "Option" menu which is only
displayed when a schematic is open. This is where I found a sub-menu
named "Set" which looks like this:
So next I clicked on the "colored background" button and changed it to
some other colour but when pressing "OK" it didn't change!?!?!
But the "Dots" and "Lines" grid allowed for changing to other colours. I
can't find anything for the "Info" function.
I've also tried the "View"-"Layers" menu (also only available when
having opened a schematic), and see that "Info" is gray for some reason,
but changing this to say, yellow doesn't make any difference. Wires are
still light green when clicking with a "Show".
If it works for you, are you on a different version/platform than me?
I'm using 6.5.0. Light on the Mac OSX platform.
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/114282
-
Re: Change "Show" highlight color?
silica10 Jun 2, 2014 6:01 PM (in response to dukepro)Maybe it's just me but I don't get it after trying just about everything within those settings.
The only thing that changes colour is the grid (just as the "Set" window says). This has to be one of the most counter-intuitive programs around if it takes all this to change a colour and I can't even find it.
-
-
-
-
Re: Change "Show" highlight color?
ezrcer May 28, 2014 8:09 PM (in response to silica10)"...So next I clicked on the "colored background" button and changed it to some other colour but when pressing "OK" it didn't change!?!?!"
Hi,
Just want to make sure that you selected an empty (gray box), select your color, and then clicked "SET COLOR" before clinking OK. in the settings menu. Then you should be able to select that color in the layer setting menu.
Sadry
-
-
Re: Change "Show" highlight color?
Autodesk Guest Jan 12, 2021 2:04 AM (in response to silica10)Am 28.05.2014 um 00:47 schrieb silica10:
Is there a way to change the "Show" function's highlight color? The
slightly lighter green when clicking on a wire doesn't make for a huge
difference from the darker green already there.
I'm using version 6.5.0. Light on a Mac.
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/114255
Hi there
First of all install version 6.6.0 because it corrects some errors in
previous versions and your license permits that.
The colours for .sch and .brd are in colour tables you can access from
sheet or board in: options/setting/colours (and background).
There is a 8X8 Matrix. The first and all uneven rows are the basic
colours, the second and all even rows are the highlight "show" colours.
I use not only highlight but contrary colours also i.e. red/green or
blue/yellow etc.
If you mix your colour don't forget to finally SET it otherwise it
wouldn't work.
After definition of colours you should test. Preferable in a sheet
because of less colours compared to a board.
Select the colour icon and double click on a colour square.
A window opens with "layer properties".
Click the colour and the colour matrix opens and (with a sharp eye) you
can see a dotted frame around one colour. That is the one you had selected.
Now you can select a new colour (the dotted frame jumps to it) and after
a couple of "OK"s the new colour is in business.
You can define all (64) colours as you want, but consider that your
colour and the background are a mix of colours and might look different
finally.
Check also "Help colours" "Help set".
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Is there a way to change the "Show" function's highlight color? The slightly lighter green when clicking on a wire doesn't make for a huge difference from the darker green already there.
I'm using version 6.5.0. Light on a Mac.