5 Replies Latest reply on Apr 7, 2021 9:23 PM by mahadeva.hn

    AXI Uart as Linux System Console

    oleb0n

      I've already tried to clarify this on xilinx forum, but it is still pending. I have several UARTs in my system, both PS and PL. The PS UARTs can be designated as petalinux system console without a problem, however every time I try to use PL UARTs for system console, the petalinux build fails with very obscure diagnostic:

       

      | make[1]: Leaving directory '/home/ob/pet_prj/h9_2/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2019.01-xilinx-v2019.2+gitAUTOINC+dc61275b1d-r0/build'

      | make: *** [Makefile:148: sub-make] Error 2

      | make: Leaving directory '/home/ob/pet_prj/h9_2/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2019.01-xilinx-v2019.2+gitAUTOINC+dc61275b1d-r0/git'

      | ERROR: oe_runmake failed

      | WARNING: exit code 1 from a shell command.

      | ERROR: Function failed: do_compile (log file is located at /home/ob/pet_prj/h9_2/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2019.01-xilinx-v2019.2+gitAUTOINC+dc61275b1d-r0/temp/log.do_compile.13996)

      ERROR: Task (/tools/Xilinx/petalinux/2019.2/components/yocto/source/aarch64/layers/meta-xilinx/meta-xilinx-bsp/recipes-bsp/u-boot/u-boot-xlnx_2019.2.bb:do_compile) failed with exit code '1'

       

      Opening the above mentioned log file gives:

       

      /home/ob/pet_prj/h9_2/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2019.01-xilinx-v2019.2+gitAUTOINC+dc61275b1d-r0/git/include/configs/platform-top.h:34:2: error: expected '}' before 'PSSERIAL0'

        PSSERIAL0 \

       

       

      I checked the file, ut does not look like I can fix it by adding a missing '}'.

      This project was build from scratch (no relicts), if I select PS_UARTx as system it builds fine. If there is a way to fix it please share

       

       

       

       

      This is complete platform-top.h:

       

      #include <configs/platform-auto.h>

       

      #define CONFIG_NR_DRAM_BANKS 3

       

      #define CONFIG_SYS_BOOTM_LEN 0xF000000

      #undef  CONFIG_SYS_BOOTMAPSZ

       

      #define DFU_ALT_INFO_RAM \

                      "dfu_ram_info=" \

              "setenv dfu_alt_info " \

              "image.ub ram $netstart 0x1e00000\0" \

              "dfu_ram=run dfu_ram_info && dfu 0 ram 0\0" \

              "thor_ram=run dfu_ram_info && thordown 0 ram 0\0"

       

      #define DFU_ALT_INFO_MMC \

              "dfu_mmc_info=" \

              "set dfu_alt_info " \

              "${kernel_image} fat 0 1\\\\;" \

              "dfu_mmc=run dfu_mmc_info && dfu 0 mmc 0\0" \

              "thor_mmc=run dfu_mmc_info && thordown 0 mmc 0\0"

       

      /*Required for uartless designs */

      #ifndef CONFIG_BAUDRATE

      #define CONFIG_BAUDRATE 115200

      #ifdef CONFIG_DEBUG_UART

      #undef CONFIG_DEBUG_UART

      #endif

      #endif

       

      /* Extra U-Boot Env settings */

      #define CONFIG_EXTRA_ENV_SETTINGS \

          SERIAL_MULTI \

          CONSOLE_ARG \

          PSSERIAL0 \

          "nc=setenv stdout nc;setenv stdin nc;\0" \

          "ethaddr=00:0a:35:00:22:01\0" \

          "importbootenv=echo \"Importing environment from SD ...\"; " \

              "env import -t ${loadbootenv_addr} $filesize\0" \

          "loadbootenv=load mmc $sdbootdev:$partid ${loadbootenv_addr} ${bootenv}\0" \

          "sd_uEnvtxt_existence_test=test -e mmc $sdbootdev:$partid /uEnv.txt\0" \

          "uenvboot=" \

              "if run sd_uEnvtxt_existence_test; then " \

                  "run loadbootenv; " \ 

                  "echo Loaded environment from ${bootenv}; " \

                  "run importbootenv; " \

              "fi\0" \

          "sdboot=echo boot Petalinux; run uenvboot ; mmcinfo && fatload mmc 0 ${netstart} ${kernel_img} && bootm \0" \

          "autoload=no\0" \

          "clobstart=0x10000000\0" \

          "netstart=0x10000000\0" \

          "dtbnetstart=0x11800000\0" \

          "loadaddr=0x10000000\0" \

          "boot_img=BOOT.BIN\0" \

          "load_boot=tftpboot ${clobstart} ${boot_img}\0" \

          "update_boot=setenv img boot; setenv psize ${bootsize}; setenv installcmd \"install_boot\"; run load_boot ${installcmd}; setenv img; setenv psize; setenv installcmd\0" \

          "install_boot=mmcinfo && fatwrite mmc 0 ${clobstart} ${boot_img} ${filesize}\0" \

          "bootenvsize=0x40000\0" \

          "bootenvstart=0x1360000\0" \

          "eraseenv=sf probe 0 && sf erase ${bootenvstart} ${bootenvsize}\0" \

          "jffs2_img=rootfs.jffs2\0" \

          "load_jffs2=tftpboot ${clobstart} ${jffs2_img}\0" \

          "update_jffs2=setenv img jffs2; setenv psize ${jffs2size}; setenv installcmd \"install_jffs2\"; run load_jffs2 test_img; setenv img; setenv psize; setenv installcmd\0" \

          "sd_update_jffs2=echo Updating jffs2 from SD; mmcinfo && fatload mmc 0:1 ${clobstart} ${jffs2_img} && run install_jffs2\0" \

          "install_jffs2=sf probe 0 && sf erase ${jffs2start} ${jffs2size} && " \

              "sf write ${clobstart} ${jffs2start} ${filesize}\0" \

          "kernel_img=image.ub\0" \

          "load_kernel=tftpboot ${clobstart} ${kernel_img}\0" \

          "update_kernel=setenv img kernel; setenv psize ${kernelsize}; setenv installcmd \"install_kernel\"; run load_kernel ${installcmd}; setenv img; setenv psize; setenv installcmd\0" \

          "install_kernel=mmcinfo && fatwrite mmc 0 ${clobstart} ${kernel_img} ${filesize}\0" \

          "cp_kernel2ram=mmcinfo && fatload mmc 0 ${netstart} ${kernel_img}\0" \

          "dtb_img=system.dtb\0" \

          "load_dtb=tftpboot ${clobstart} ${dtb_img}\0" \

          "update_dtb=setenv img dtb; setenv psize ${dtbsize}; setenv installcmd \"install_dtb\"; run load_dtb test_img; setenv img; setenv psize; setenv installcmd\0" \

          "sd_update_dtb=echo Updating dtb from SD; mmcinfo && fatload mmc 0:1 ${clobstart} ${dtb_img} && run install_dtb\0" \

          "fault=echo ${img} image size is greater than allocated place - partition ${img} is NOT UPDATED\0" \

          "test_crc=if imi ${clobstart}; then run test_img; else echo ${img} Bad CRC - ${img} is NOT UPDATED; fi\0" \

          "test_img=setenv var \"if test ${filesize} -gt ${psize}\\; then run fault\\; else run ${installcmd}\\; fi\"; run var; setenv var\0" \

          "netboot=tftpboot ${netstart} ${kernel_img} && bootm\0" \

          "default_bootcmd=run cp_kernel2ram && bootm ${netstart}\0" \

      ""

        • Re: AXI Uart as Linux System Console
          mahadeva.hn

          Hi,

           

          I'm also facing the same problem, when I import custom HDF file. Please help me with the solution.

            • Re: AXI Uart as Linux System Console
              drozwood90

              Hi there,

               

              What system are you using?

               

              --Dan

                • Re: AXI Uart as Linux System Console
                  mahadeva.hn

                  I am using Ultrazed-3EG IOCC board.

                  petalinux version: 2018.3

                   

                  In file included from include/config.h:5:0,

                                   from /media/mahadeva/ubuntu_data/ultrazed/iocc_linux/uz3eg_iocc_dp_2018_3/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2018.01-xilinx-v2018.3+gitAUTOINC+d8fc4b3b70-r0/git/arch/arm/include/asm/string.h:4,

                                   from /media/mahadeva/ubuntu_data/ultrazed/iocc_linux/uz3eg_iocc_dp_2018_3/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2018.01-xilinx-v2018.3+gitAUTOINC+d8fc4b3b70-r0/git/include/linux/string.h:21,

                                   from /media/mahadeva/ubuntu_data/ultrazed/iocc_linux/uz3eg_iocc_dp_2018_3/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2018.01-xilinx-v2018.3+gitAUTOINC+d8fc4b3b70-r0/git/include/common.h:30,

                                   from /media/mahadeva/ubuntu_data/ultrazed/iocc_linux/uz3eg_iocc_dp_2018_3/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2018.01-xilinx-v2018.3+gitAUTOINC+d8fc4b3b70-r0/git/env/common.c:11:

                  /media/mahadeva/ubuntu_data/ultrazed/iocc_linux/uz3eg_iocc_dp_2018_3/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2018.01-xilinx-v2018.3+gitAUTOINC+d8fc4b3b70-r0/git/include/configs/platform-top.h:6:2: error: expected '}' before 'SERIAL_MULTI'

                    SERIAL_MULTI\

                    ^

                  /media/mahadeva/ubuntu_data/ultrazed/iocc_linux/uz3eg_iocc_dp_2018_3/build/tmp/work/plnx_zynqmp-xilinx-linux/u-boot-xlnx/v2018.01-xilinx-v2018.3+gitAUTOINC+d8fc4b3b70-r0/git/include/configs/platform-top.h:6:2: note: in definition of macro 'CONFIG_EXTRA_ENV_SETTINGS'

                    SERIAL_MULTI\

                    ^~~~~~~~~~~~~

                    CONSOLE_ARG\